S32K v3.0.0 and R2017b license error solved

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K v3.0.0 and R2017b license error solved

1,886件の閲覧回数
lethuer2
Contributor II

Hello dumitru-daniel.popa‌

first time I have a tipp for you !

Like discussed here https://community.nxp.com/thread/467938#comment-980540 I wanted to use S32Kv3.0.0 toolbox with R2017b and got this license error:

Unbenannt.PNG

I made all the steps recommended and completely new downloaded and installed the toolbox.

- I generated a new license file and saved it with the file extension .lic to the installation folder

- RESET the MATLAB default paths to DEFAULT using the Set Path menu to remove all previous toolboxes

- run the mbd_s32K_path.m to add the S32K1xx into MATLAB

- added the lic folder manually to the Matlab paths

In opposite to v2.0 (which does not work with R2017b) I was not able to change the path during installation of v3.0.

So now I simply copied the installed content of v3.0 toolbox from the automatic generated path to a different folder and that solved the problem after simply running the mbd_s32K_path.m again.

Maybe the standard installation path was too long or the space in my username leads to some problems so the lic file couldn't be found. 

Anyway...

Best regards

Leon

0 件の賞賛
返信
1 返信

1,698件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Leon, 

Thank you for reporting this and glad to find out you have resolved.

You can change the default Add-Ons installation paths directly from MATLAB Preferences before Toolbox install.

pastedImage_1.png

Best regards,

Daniel

0 件の賞賛
返信