S32K PIL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K PIL

1,623 Views
MinaNaguib
Contributor I

Hi Everyone,

I am trying to run PIL with S32K board and Simulink. I just want to run a function that takes 300 inputs and produce 100 outputs in double format. My objective is to benchmark the performance of the processor running this algorithm in the loop. My question is do NXP support this with Simulink ? and do I need extra components besides the S32K board i.e., connections or any other?. 

Thanks 

0 Kudos
Reply
1 Reply

1,602 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @MinaNaguib ,

Yes, NXP supports running PIL on the S32K1xx board. We also provide some PIL example in our toolbox so I think they are a good starting point.

Hope this helps,

Marius

0 Kudos
Reply