S32K PIL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K PIL

1,638件の閲覧回数
MinaNaguib
Contributor I

Hi Everyone,

I am trying to run PIL with S32K board and Simulink. I just want to run a function that takes 300 inputs and produce 100 outputs in double format. My objective is to benchmark the performance of the processor running this algorithm in the loop. My question is do NXP support this with Simulink ? and do I need extra components besides the S32K board i.e., connections or any other?. 

Thanks 

0 件の賞賛
返信
1 返信

1,617件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @MinaNaguib ,

Yes, NXP supports running PIL on the S32K1xx board. We also provide some PIL example in our toolbox so I think they are a good starting point.

Hope this helps,

Marius

0 件の賞賛
返信