S32K MBDT version 1.6 vs 1.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K MBDT version 1.6 vs 1.4

681 Views
andrewmer
Contributor I

Hi, I am attempting to use version 1.4 of the MBDT S32K add-on for MATLAB with the S32k3XEVB-T172 and running into issues. I am specifically trying to use version 1.4 of the tool because I would like to evaluate the BMS add-on but have been unable to get any of the provided examples to run in version 1.4 of the tool.  However, using version 1.6 of the add-on I have had no issues. The example I have been using is: 

MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K3xx\S32K3_Examples\dio\s32k3xx_dio_s32ct\s32k3xx_dio_s32ct.mdl

In both versions of the add-on, for this specific example I update the hardware part to be the S32K344-Q172 and set the configuration template to be s32_default_project_config for the S32k344-Q172. See attached.  After making the one small change can hit build, and in Version 1.6 of the add-on everything works as expected.  However, using version 1.4 of the tool when I hit build I get no build errors or anything indicating there is an issue, the firmware updates and the board restarts yet the example does not run instead D3 on the eval board becomes constantly lit.

Tags (1)
0 Kudos
Reply
1 Reply

552 Views
dragostoma
NXP Employee
NXP Employee

Hi, @andrewmer,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

What is the current status of your issue? Are you still experiencing this problem? It is possible that both versions of the toolbox were present in the MATLAB path, which could have caused conflicts. Which version of MATLAB are you using?

We will try to reproduce your issue, but an updated status and details on your progress would be helpful.

 

Best regards,

Dragos

0 Kudos
Reply