Multiple CAN receive issue MBDT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple CAN receive issue MBDT

938 Views
MReza
Contributor II

Hi everyone!

I'm working on a project using MBDT for K358BMU and mc33774a and I need some help or reference with configuring the CAN Receive block to handle multiple message IDs properly. This is my setup as of now

image.png

image.png

I was trying this out after seeing another community post with this solution, but it dint seem to work for me.

Also how do you select the hardware object for CAN receive, because for can_write blocks it is straightforward, am i missing something?

image.png

If anyone has experience or some idea about this could share a working example model with CAN receive and multiple ID handling or point me in the right direction! thanks

Tags (5)
0 Kudos
Reply
0 Replies