S32 Design Studio for ARM 2018.R1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for ARM 2018.R1

1,970 Views
hayaoki7
Contributor IV

Can I use S32 Design Studio for ARM 2018.R1 with MBD toolbox S32K 3.0

Best regards

1 Reply

1,808 Views
constantinrazva
NXP Employee
NXP Employee

Hello hayaoki7‌,

Yes, you can use MBDT 3.0 with S32 Design Studio for ARM 2018.R1.

To import a project generated by our toolbox, go to Import and select ProjectInfo.xlm Importer (shown below):

pastedImage_1.png

You have to browse to the folder generated by the toolbox and select the ProjectInfo.xml file.

pastedImage_3.png

After that, you are all set. All you have to do is build the project and configure (if needed) options for the debugger (from Debug Configurations).

Please let us know if you need further help with this.

Kind regards,

Razvan.