[S12Z Toolbox version 1.4] Example model causes matlab crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S12Z Toolbox version 1.4] Example model causes matlab crash

13,751 Views
nofake_drstrang
Contributor III

Dear Team,

I have successfully installed the new toolbox version 1.4 for S12Z.

The bootloader version 1.6.2.14 is not up to date in the folfer "\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\tools\BootLoader"

So I install the new version 1.6.7.35.

Firstly I tried with the example "MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\adc\adc_s12zvm.mdl".

After some adaptions on COM-port in "Configuration Parameters/PIL and Download Config", I can build successfully and download the application. The LED blinks.

Now I try with the next example model "\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_ClosedLoop_Sensorless_S12ZVM.mdl" 

Because of too long name, there is a build error: "Build failed because the build file name(s) exceed the Windows limit of 260 characters"

So I change to a shorter name "PMSM_Sensless.mdl". 

But Matlab crashes everytime I tried to build the model. (Simulation works without errors)

Please see the attached crash-report (crash_report.txt not allowed, so I do a zip)

Environment:

S12ZVMx12EVB

Microsoft Windows 7 Ultimate / 64bit

MATLAB Version 9.8 (R2020a)
Simulink Version 10.1 (R2020a)
Embedded Coder Version 7.4 (R2020a)
MATLAB Coder Version 5.0 (R2020a)
MATLAB Compiler Version 8.0 (R2020a)
MATLAB Compiler SDK Version 6.8 (R2020a)
Model-Based Design Toolbox for S12ZVMx Series Version 1.4.0 (R2015a-R2020a)
Simulink Coder Version 9.3 (R2020a)
Simulink Compiler Version 1.0 (R2020a)
Stateflow Version 10.2 (R2020a)

Matlab_crash.PNG

 

Please help me!

Thanks in advance!

0 Kudos
Reply
19 Replies

13,379 Views
nofake_drstrang
Contributor III

Hi @adriantudor @paulvlase 

we have had to update to matlab 2020b. And it works finally, no matlab crash any more !

One question please:

In the example model, is there a swap?

angleVertausch.PNG

 

And why do the parameters (Ramp Up/Down) not have interger (f16) values?

wrongPara.PNG 

But somehow the motor spins...

Many thanks!

0 Kudos
Reply

13,435 Views
nofake_drstrang
Contributor III

Hi @adriantudor @paulvlase 

actually I posted it 3 hours ago. But somehow now I can not see it in the forum. I post it again...

I keep trying hard to make the demo "PMSM_ClosedLoop" run, but until now without success...

Step 1:

From the original demo model, I comment out both the blocks "FOC" and "PosObserver". It builds successfully, without any errors.

FocObs_Auskommen_OK.png

 

Step 2:

Activate only  "PosObserver" ("FOC" commented out). Replace with blocks from lib: "AMCLIB_BemfObsrvDQ_F16" and "AMCLIB_TrackObsrv_F16" and changes names to shorter names "BemfObsrvDQ" and "TrackObsrv":

Obs_NOK.png

 

Build warnings/errors:

=== Build (Elapsed: 45 sec) ===
### Starting build procedure for: PMSM_Sensorless
### Generating code and artifacts to 'Model specific' folder structure
### Generating code into build folder: D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pIAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pIAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pUAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pUAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:Warning: File 'codedescriptor.dmr' not found.
Warning:Warning: File 'codedescriptor.dmr' not found.
Warning:Warning: File 'codedescriptor.dmr' not found.
Warning:Warning: File 'codedescriptor.dmr' not found.
### Invoking Target Language Compiler on PMSM_Sensorless.rtw
### Using System Target File: D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tlc
### Loading TLC function libraries
### Generating TLC interface API for custom data
### Initial pass through model to cache user defined code
### Caching model source code
...............................................................................
...............................................................................
.................................................
### Writing header file PMSM_Sensorless_types.h
### Writing source file PMSM_Sensorless.c
### Writing header file PMSM_Sensorless_private.h
### Writing header file PMSM_Sensorless.h
.
### Writing source file profile_buffer.c
### Writing header file profile_buffer.h
### Writing header file rtwtypes.h
### Writing header file zero_crossing_types.h
### Writing source file PMSM_Sensorless_FastLoopOutput.c
.
### Writing source file PosObserver.c
### Writing source file FastLoopAlgorithm.c
### Writing source file FastLoopInput.c
### Writing source file PositionMode.c
### Writing source file SlowLoopAlgorithm.c
### Writing header file PMSM_Sensorless_FastLoopOutput.h
.
### Writing header file PosObserver.h
### Writing header file FastLoopAlgorithm.h
### Writing header file FastLoopInput.h
### Writing header file PositionMode.h
### Writing header file SlowLoopAlgorithm.h
.
### Writing source file PMSM_Sensorless_data.c
### Writing header file mc9s12zvm.h
### Writing header file tim_param.h
### Writing header file fm_data_rec.h
### Writing source file mcd_main.c
.
### Writing header file clk_init.h
### Writing header file vector.h
### Writing header file isr_lvl.h
### Writing source file isr_lvl.c
### TLC code generation complete.
.### Evaluating PostCodeGenCommand specified in the model
.
### Processing Template Makefile: D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf
Warning:Found legacy make variables |>START_MDLREFINC_EXPAND_INCLUDES<|, |>END_MDLREFINC_EXPAND_INCLUDES<|, |>MODELREF_INC_PATH<| in the template makefile D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf. The variables are no longer required. You can remove the variables.
### Creating D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw\PMSM_Sensorless.mk from D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf
### Building PMSM_Sensorless: .\PMSM_Sensorless.bat
### Build procedure for PMSM_Sensorless aborted due to an error.
Warning:Found legacy make variables |>S_FUNCTIONS<|, |>S_FUNCTIONS_OBJ<| in the template makefile D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf. The variables are no longer required. You can remove the variables.
Warning:Found legacy make variables |>SHARED_BIN_DIR<|, |>SHARED_LIB<|, |>SHARED_SRC<|, |>SHARED_SRC_DIR<| in the template makefile D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf. The variables are no longer required. You can remove the variables.
Error:
D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw>set MATLAB=D:\matlab2020a

D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw>"D:\matlab2020a\bin\win64\gmake" -f PMSM_Sensorless.mk COPY_MDLREF_INCLUDES=0 GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 CW_TARGET_DEFAULT_LCF=1 CW_TARGET_USER_LCF="mc9s12zvml128_FLASH.prm" CS_TARGET_DEFAULT_LCF=1 CS_TARGET_USER_LCF="mc9s12zvm32_FLASH.lkf" PIL_DOWNLOAD=0 RBL_DOWNLOAD=1 ISPROTECTINGMODEL=NOTPROTECTING OPTS="-DTID01EQ=0"
Cleaning...
RELATIVE_PATH_TO_ANCHOR is ..
==== Removing object files from build directory ====
Compiler details : "C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -c -model small -bfield_lsbit_first -bfield_reduce_type -opt level=2 -opt speed -inline auto -requireprotos -Cpp_Exceptions off -char unsigned -msgstyle parseable -sym full -nostdinc -nosyspath -w possible -w extended -w extracomma -w emptydecl -w structclass -ansi off -ipa function -inline smart,auto,bottomup -bool off -wchar_t off -RTTI off -llong_size=8 -double_size 8 -lang c99 -gccext on -o SetupFiles -I. -I.. -I../instrumented -I.. -I"D:\matlab2020a\simulink\include" -I"D:\matlab2020a\extern\include" -I"D:\matlab2020a\rtw\c\src" -I"D:\matlab2020a\rtw\c\libsrc" -I"D:\matlab2020a\rtw\c\src\ext_mode\common" -I"D:\matlab2020a\rtw\c\src\ext_mode\tcpip" -I"D:\matlab2020a\rtw\c\src\ext_mode\serial" -I"D:\matlab2020a\rtw\c\src\ext_mode\custom" -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw -ID:\matlab2020a\extern\include -ID:\matlab2020a\simulink\include -ID:\matlab2020a\rtw\c\src -ID:\matlab2020a\rtw\c\src\ext_mode\common -ID:\matlab2020a\rtw\c\ert -I"C:/Freescale/Codewarrior_11\MCU\S12lisa_Support\s12lisac\include" -DTID01EQ=0
Assembler details : "C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -CMacAngBrackOn -ViewHidden
Product: PMSM_Sensorless.elf
Build product type: executable
Building file FastLoopAlgorithm.o...
"C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -c -model small -bfield_lsbit_first -bfield_reduce_type -opt level=2 -opt speed -inline auto -requireprotos -Cpp_Exceptions off -char unsigned -msgstyle parseable -sym full -nostdinc -nosyspath -w possible -w extended -w extracomma -w emptydecl -w structclass -ansi off -ipa function -inline smart,auto,bottomup -bool off -wchar_t off -RTTI off -llong_size=8 -double_size 8 -lang c99 -gccext on -o FastLoopAlgorithm.o -I. -I.. -I../instrumented -I.. -I"D:\matlab2020a\simulink\include" -I"D:\matlab2020a\extern\include" -I"D:\matlab2020a\rtw\c\src" -I"D:\matlab2020a\rtw\c\libsrc" -I"D:\matlab2020a\rtw\c\src\ext_mode\common" -I"D:\matlab2020a\rtw\c\src\ext_mode\tcpip" -I"D:\matlab2020a\rtw\c\src\ext_mode\serial" -I"D:\matlab2020a\rtw\c\src\ext_mode\custom" -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw -ID:\matlab2020a\extern\include -ID:\matlab2020a\simulink\include -ID:\matlab2020a\rtw\c\src -ID:\matlab2020a\rtw\c\src\ext_mode\common -ID:\matlab2020a\rtw\c\ert -I"C:/Freescale/Codewarrior_11\MCU\S12lisa_Support\s12lisac\include" -DTID01EQ=0 FastLoopAlgorithm.c
C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa|Compiler|Error
(D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw\FastLoopAlgorithm.h|26|9|10|811|10)
=#include "gmclib.h"
>the file 'gmclib.h' cannot be opened

Errors caused tool to abort.
gmake: *** [FastLoopAlgorithm.o] Error 1

Error(s) encountered while building "PMSM_Sensorless"

Step 3:

Comment out "AMCLIB_BemfObsrvDQ_F16"

BemfObs_cmtOut.png

Build successfully, no errors.

Do you have any ideas, what I could do?

Many thanks in advance!

0 Kudos
Reply

13,424 Views
nofake_drstrang
Contributor III

Hi @adriantudor @paulvlase 

I keep trying...

Step 1:

Because with the example model "PMSM_ClosedLoop", when I comment out both the "FOC" and " PosObserver"-Blocks, then I can build the model successfully:

Without FOC/Observer: OKWithout FOC/Observer: OK

 

Step 2: 

Firstly activate only the "PosObserver", but remodeling with the lib-bocks: "AMCLIB_BemfObsrvDQ_F16" and "AMCLIB_TrackObsrv_F16". Name changes to shorter names: "BemfObsrvDQ" and "TrackObsrv":

Remodeling of ObserverRemodeling of Observer

Build errors:

 

=== Build (Elapsed: 45 sec) ===
### Starting build procedure for: PMSM_Sensorless
### Generating code and artifacts to 'Model specific' folder structure
### Generating code into build folder: D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pIAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pIAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pUAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/pUAB' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal1' does not match the name 'SWLIBS_2Syst_F16.f16Arg1' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:The input bus to block 'PMSM_Sensorless/FastLoopAlgorithm/PosObserver/BemfObsrvDQ/AMCLIB_BemfObsrvDQ_SF' does not match the bus specified by the bus object 'SWLIBS_2Syst_F16' on the block dialog : Signal 'signal2' does not match the name 'SWLIBS_2Syst_F16.f16Arg2' of the corresponding bus element in the bus object. To disable this diagnostic, set the Configuration Parameters > Diagnostics > Connectivity > 'Element name mismatch' option to 'None'.
Warning:Warning: File 'codedescriptor.dmr' not found.
Warning:Warning: File 'codedescriptor.dmr' not found.
Warning:Warning: File 'codedescriptor.dmr' not found.
Warning:Warning: File 'codedescriptor.dmr' not found.
### Invoking Target Language Compiler on PMSM_Sensorless.rtw
### Using System Target File: D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tlc
### Loading TLC function libraries
### Generating TLC interface API for custom data
### Initial pass through model to cache user defined code
### Caching model source code
...............................................................................
...............................................................................
.................................................
### Writing header file PMSM_Sensorless_types.h
### Writing source file PMSM_Sensorless.c
### Writing header file PMSM_Sensorless_private.h
### Writing header file PMSM_Sensorless.h
.
### Writing source file profile_buffer.c
### Writing header file profile_buffer.h
### Writing header file rtwtypes.h
### Writing header file zero_crossing_types.h
### Writing source file PMSM_Sensorless_FastLoopOutput.c
.
### Writing source file PosObserver.c
### Writing source file FastLoopAlgorithm.c
### Writing source file FastLoopInput.c
### Writing source file PositionMode.c
### Writing source file SlowLoopAlgorithm.c
### Writing header file PMSM_Sensorless_FastLoopOutput.h
.
### Writing header file PosObserver.h
### Writing header file FastLoopAlgorithm.h
### Writing header file FastLoopInput.h
### Writing header file PositionMode.h
### Writing header file SlowLoopAlgorithm.h
.
### Writing source file PMSM_Sensorless_data.c
### Writing header file mc9s12zvm.h
### Writing header file tim_param.h
### Writing header file fm_data_rec.h
### Writing source file mcd_main.c
.
### Writing header file clk_init.h
### Writing header file vector.h
### Writing header file isr_lvl.h
### Writing source file isr_lvl.c
### TLC code generation complete.
.### Evaluating PostCodeGenCommand specified in the model
.
### Processing Template Makefile: D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf
Warning:Found legacy make variables |>START_MDLREFINC_EXPAND_INCLUDES<|, |>END_MDLREFINC_EXPAND_INCLUDES<|, |>MODELREF_INC_PATH<| in the template makefile D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf. The variables are no longer required. You can remove the variables.
### Creating D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw\PMSM_Sensorless.mk from D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf
### Building PMSM_Sensorless: .\PMSM_Sensorless.bat
### Build procedure for PMSM_Sensorless aborted due to an error.
Warning:Found legacy make variables |>S_FUNCTIONS<|, |>S_FUNCTIONS_OBJ<| in the template makefile D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf. The variables are no longer required. You can remove the variables.
Warning:Found legacy make variables |>SHARED_BIN_DIR<|, |>SHARED_LIB<|, |>SHARED_SRC<|, |>SHARED_SRC_DIR<| in the template makefile D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\mctbx_s12zvm\mctbx_s12zvm\mcd_s12zvm.tmf. The variables are no longer required. You can remove the variables.
Error:
D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw>set MATLAB=D:\matlab2020a

D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw>"D:\matlab2020a\bin\win64\gmake" -f PMSM_Sensorless.mk COPY_MDLREF_INCLUDES=0 GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 CW_TARGET_DEFAULT_LCF=1 CW_TARGET_USER_LCF="mc9s12zvml128_FLASH.prm" CS_TARGET_DEFAULT_LCF=1 CS_TARGET_USER_LCF="mc9s12zvm32_FLASH.lkf" PIL_DOWNLOAD=0 RBL_DOWNLOAD=1 ISPROTECTINGMODEL=NOTPROTECTING OPTS="-DTID01EQ=0"
Cleaning...
RELATIVE_PATH_TO_ANCHOR is ..
==== Removing object files from build directory ====
Compiler details : "C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -c -model small -bfield_lsbit_first -bfield_reduce_type -opt level=2 -opt speed -inline auto -requireprotos -Cpp_Exceptions off -char unsigned -msgstyle parseable -sym full -nostdinc -nosyspath -w possible -w extended -w extracomma -w emptydecl -w structclass -ansi off -ipa function -inline smart,auto,bottomup -bool off -wchar_t off -RTTI off -llong_size=8 -double_size 8 -lang c99 -gccext on -o SetupFiles -I. -I.. -I../instrumented -I.. -I"D:\matlab2020a\simulink\include" -I"D:\matlab2020a\extern\include" -I"D:\matlab2020a\rtw\c\src" -I"D:\matlab2020a\rtw\c\libsrc" -I"D:\matlab2020a\rtw\c\src\ext_mode\common" -I"D:\matlab2020a\rtw\c\src\ext_mode\tcpip" -I"D:\matlab2020a\rtw\c\src\ext_mode\serial" -I"D:\matlab2020a\rtw\c\src\ext_mode\custom" -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw -ID:\matlab2020a\extern\include -ID:\matlab2020a\simulink\include -ID:\matlab2020a\rtw\c\src -ID:\matlab2020a\rtw\c\src\ext_mode\common -ID:\matlab2020a\rtw\c\ert -I"C:/Freescale/Codewarrior_11\MCU\S12lisa_Support\s12lisac\include" -DTID01EQ=0
Assembler details : "C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -CMacAngBrackOn -ViewHidden
Product: PMSM_Sensorless.elf
Build product type: executable
Building file FastLoopAlgorithm.o...
"C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -c -model small -bfield_lsbit_first -bfield_reduce_type -opt level=2 -opt speed -inline auto -requireprotos -Cpp_Exceptions off -char unsigned -msgstyle parseable -sym full -nostdinc -nosyspath -w possible -w extended -w extracomma -w emptydecl -w structclass -ansi off -ipa function -inline smart,auto,bottomup -bool off -wchar_t off -RTTI off -llong_size=8 -double_size 8 -lang c99 -gccext on -o FastLoopAlgorithm.o -I. -I.. -I../instrumented -I.. -I"D:\matlab2020a\simulink\include" -I"D:\matlab2020a\extern\include" -I"D:\matlab2020a\rtw\c\src" -I"D:\matlab2020a\rtw\c\libsrc" -I"D:\matlab2020a\rtw\c\src\ext_mode\common" -I"D:\matlab2020a\rtw\c\src\ext_mode\tcpip" -I"D:\matlab2020a\rtw\c\src\ext_mode\serial" -I"D:\matlab2020a\rtw\c\src\ext_mode\custom" -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop -ID:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw -ID:\matlab2020a\extern\include -ID:\matlab2020a\simulink\include -ID:\matlab2020a\rtw\c\src -ID:\matlab2020a\rtw\c\src\ext_mode\common -ID:\matlab2020a\rtw\c\ert -I"C:/Freescale/Codewarrior_11\MCU\S12lisa_Support\s12lisac\include" -DTID01EQ=0 FastLoopAlgorithm.c
C:/Freescale/Codewarrior_11/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa|Compiler|Error
(D:\MATLAB\AddOns\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop\PMSM_Sensorless_mbd_rtw\FastLoopAlgorithm.h|26|9|10|811|10)
=#include "gmclib.h"
>the file 'gmclib.h' cannot be opened

Errors caused tool to abort.
gmake: *** [FastLoopAlgorithm.o] Error 1

Error(s) encountered while building "PMSM_Sensorless"

 

Do you have any ideas, what I could try?

Thanks in Advance!

Best regards.

please find the attached model.

0 Kudos
Reply

13,695 Views
nofake_drstrang
Contributor III

Hi @adriantudor 

I have recently tried to build the example: "\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\BLDC_Demo\BLDC_ClosedLoop\BLDC_ClosedLoop_S12ZVM.mdl"

It works without any errors!

0 Kudos
Reply

13,741 Views
adriantudor
NXP Employee
NXP Employee

Hi @nofake_drstrang ,

 

I tried to build this example on my machine and it's ok. I recommend you to copy the "PMSM_ClosedLoop"  folder on your root (eg.: C:\PMSM_ClosedLoop). Be sure that the folder copied is not protected and it can be written (check in the folder proprieties). Then add this folder to the path using Matlab, then try to build it.

 

Best regards,

Adrian

0 Kudos
Reply

13,566 Views
nofake_drstrang
Contributor III

Hi @adriantudor 

could you please share your working model ? 

 

Many thanks in advance! 

0 Kudos
Reply

13,550 Views
adriantudor
NXP Employee
NXP Employee

@nofake_drstrang  Hi,

 

Here is my working PMSM ZVM model.

Please let me know if this one it works for you.

 

Best regards,

Adrian

0 Kudos
Reply

13,539 Views
nofake_drstrang
Contributor III

Hi @adriantudor,

many thanks!

 

Unfortunately it does not work

But when I comment out the FOC- and Observer- Blocks, then It works without crash.

I have Simulink/matlab 2020a. Your model is saved in R2019.

 

Foc_Obs_commentOut.PNG

Many thanks!

0 Kudos
Reply

13,528 Views
adriantudor
NXP Employee
NXP Employee

@nofake_drstrang  Hi,

 

Try to reduce the length of the names of all blocks/subsystems that are included in the FOC- and Observer- Blocks (and even the names of those 2 blocks). Unfortunately, I can't try that on my machine because I don't have this issue. And please let me know if it works.

 

Thank you,

Adrian

0 Kudos
Reply

13,507 Views
nofake_drstrang
Contributor III

Hi @adriantudor 

 

I tried but unfortunately it did not work. Same crash...

 

0 Kudos
Reply

13,609 Views
nofake_drstrang
Contributor III

Hi @adriantudor 

could you please share your working model? 

 

Many thanks! 

0 Kudos
Reply

13,725 Views
nofake_drstrang
Contributor III

Hello @adriantudor ,

thanks for your reply!

 

I tried your suggestion, but same crash...

writeprotect.PNGsetpath.PNGMatlab_crash2.PNG

 

Crash Report:

MATLAB crash file:D:\TEMP\matlab_crash_dump.5236-1:


--------------------------------------------------------------------------------
Access violation detected at Fr Sep 11 02:34:35 2020 +0200
--------------------------------------------------------------------------------

Configuration:
Crash Decoding : Disabled - No sandbox or build area path
Crash Mode : continue (default)
Default Encoding : windows-1252
Deployed : false
Graphics Driver : Unknown hardware
Graphics card 1 : NVIDIA ( 0x10de ) NVIDIA GeForce GTX 460 Version 10.18.13.5582 (2015-8-25)
Java Version : Java 1.8.0_202-b08 with Oracle Corporation Java HotSpot(TM) 64-Bit Server VM mixed mode
MATLAB Architecture : win64
MATLAB Entitlement ID : 6257193
MATLAB Root : C:\Program Files\MATLAB\R2020a
MATLAB Version : 9.8.0.1323502 (R2020a)
OpenGL : hardware
Operating System : Microsoft Windows 7 Ultimate
Process ID : 5236
Processor ID : x86 Family 6 Model 42 Stepping 7, GenuineIntel
Session Key : 5d89cee5-8153-411a-a8a1-62f21120602f
Window System : Version 6.1 (Build 7601: Service Pack 1)

Fault Count: 1


Abnormal termination:
Access violation

Register State (from fault):
RAX = 000000011da681d0 RBX = 0000000000000040
RCX = 0000000000000000 RDX = 0000000000000000
RSP = 00000000093a4690 RBP = 00000000c0f7ee20
RSI = 00000000093a4878 RDI = 000000011da681d0

R8 = 00000000b4349720 R9 = 00000000c0f7ee20
R10 = 0000000000000000 R11 = 00000000093a4490
R12 = 0000000000000000 R13 = 00000000c0f70de0
R14 = 0000000000000040 R15 = 0000000000000000

RIP = 000007fe76ca1f4c EFL = 00010202

CS = 0033 FS = 0053 GS = 002b

Stack Trace (from fault):
[ 0] 0x000007fe76ca1f4c C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00597836 SLCG::SignalBase::isForChecksum+00003852
[ 1] 0x000007fe76ca1508 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00595208 SLCG::SignalBase::isForChecksum+00001224
[ 2] 0x000007fe76c9ace4 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00568548 mwboost::serialization::singleton_module::lock+00001092
[ 3] 0x000007fe76c9ab53 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00568147 mwboost::serialization::singleton_module::lock+00000691
[ 4] 0x000007fe76caac66 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00633958 SLCG::createCompiledSystems+00021302
[ 5] 0x000007fe76ca6322 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00615202 SLCG::createCompiledSystems+00002546
[ 6] 0x000007fe76ca6894 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00616596 SLCG::createCompiledSystems+00003940
[ 7] 0x000007fe76ca61d5 C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00614869 SLCG::createCompiledSystems+00002213
[ 8] 0x000007fe76ca5aeb C:\Program Files\MATLAB\R2020a\bin\win64\slcg_impl.dll+00613099 SLCG::createCompiledSystems+00000443
[ 9] 0x000007fe83d26479 C:\Program Files\MATLAB\R2020a\bin\win64\libmwsimulink.dll+10445945 RTWCG::RTWContextImpl::PopulateVarGroupIF::useRootOutportBuffer+00220921
[ 10] 0x000007fe83d2f33f C:\Program Files\MATLAB\R2020a\bin\win64\libmwsimulink.dll+10482495 RTWCG::RTWContextImpl::PopulateVarGroupIF::useRootOutportBuffer+00257471
[ 11] 0x000007fe83a64930 C:\Program Files\MATLAB\R2020a\bin\win64\libmwsimulink.dll+07555376 slFullGetParam+00003200
[ 12] 0x000007fec1c5b3bc bin\win64\pgo\m_dispatcher.dll+00046012 Mfh_MATLAB_fn_impl::dispatch_mf_with_reuse+00000172
[ 13] 0x000007fec1c61f12 bin\win64\pgo\m_dispatcher.dll+00073490 Mlm_file::needToCheckoutLicense+00002674
[ 14] 0x000007fec1c6143d bin\win64\pgo\m_dispatcher.dll+00070717 Mfh_MATLAB_fn_impl::dispatch+00000045
[ 15] 0x000007febe504002 bin\win64\pgo\m_lxe.dll+00540674
[ 16] 0x000007febe501ce4 bin\win64\pgo\m_lxe.dll+00531684
[ 17] 0x000007febe5e0179 bin\win64\pgo\m_lxe.dll+01442169 MathWorks::lxe::StartupLxeEngine+00239509
[ 18] 0x000007febe4f3f8d bin\win64\pgo\m_lxe.dll+00475021
[ 19] 0x000007febe4f6344 bin\win64\pgo\m_lxe.dll+00484164
[ 20] 0x000007febe4f745d bin\win64\pgo\m_lxe.dll+00488541
[ 21] 0x000007febe4f704f bin\win64\pgo\m_lxe.dll+00487503
[ 22] 0x000007febe600fb4 bin\win64\pgo\m_lxe.dll+01576884 MathWorks::lxe::StartupLxeEngine+00374224
[ 23] 0x000007febe4ff30b bin\win64\pgo\m_lxe.dll+00520971
[ 24] 0x000007febe4f562e bin\win64\pgo\m_lxe.dll+00480814
[ 25] 0x000007febe4f4358 bin\win64\pgo\m_lxe.dll+00475992
[ 26] 0x000007febe4f3fdc bin\win64\pgo\m_lxe.dll+00475100
[ 27] 0x000007fec1c625d0 bin\win64\pgo\m_dispatcher.dll+00075216 AutoPushingExecutionFrame::~AutoPushingExecutionFrame+00000784
[ 28] 0x000007fec1c6226d bin\win64\pgo\m_dispatcher.dll+00074349 Mfh_file::dispatch_with_reuse+00000045
[ 29] 0x000007feb9a73c0e bin\win64\pgo\mcos_impl.dll+00539662 mdIsA+00084078
[ 30] 0x000007feb9a7419e bin\win64\pgo\mcos_impl.dll+00541086 mdIsA+00085502
[ 31] 0x000007feb9a69cf3 bin\win64\pgo\mcos_impl.dll+00498931 mdIsA+00043347
[ 32] 0x000007feb9a6a4f3 bin\win64\pgo\mcos_impl.dll+00500979 mdIsA+00045395
[ 33] 0x000007feb9a6b6d5 bin\win64\pgo\mcos_impl.dll+00505557 mdIsA+00049973
[ 34] 0x000007feb9a94412 bin\win64\pgo\mcos_impl.dll+00672786 mdIsA+00217202
[ 35] 0x000007fec1c642fc bin\win64\pgo\m_dispatcher.dll+00082684 mdWhichInfo::fill_hidden_and_non_contextual+00006444
[ 36] 0x000007fec1c644d9 bin\win64\pgo\m_dispatcher.dll+00083161 Mfh_MATLAB_fn_impl::dispatch_with_reuse+00000045
[ 37] 0x000007febe50317b bin\win64\pgo\m_lxe.dll+00536955
[ 38] 0x000007febe500d47 bin\win64\pgo\m_lxe.dll+00527687
[ 39] 0x000007febe612c65 bin\win64\pgo\m_lxe.dll+01649765 MathWorks::lxe::ShutdownLxeEngine+00057593
[ 40] 0x000007febe612b8f bin\win64\pgo\m_lxe.dll+01649551 MathWorks::lxe::ShutdownLxeEngine+00057379
[ 41] 0x000007febe6129c3 bin\win64\pgo\m_lxe.dll+01649091 MathWorks::lxe::ShutdownLxeEngine+00056919
[ 42] 0x000007febe501ce4 bin\win64\pgo\m_lxe.dll+00531684
[ 43] 0x000007febe63ad51 bin\win64\pgo\m_lxe.dll+01813841 mwboost::archive::detail::oserializer<mwboost::archive::binaryTerm_oarchive,ir::IrTree>::oserializer<mwboost::archive::binaryTerm_oarchive,ir::IrTree>+00059517
[ 44] 0x000007febe4f3f8d bin\win64\pgo\m_lxe.dll+00475021
[ 45] 0x000007febe4f6344 bin\win64\pgo\m_lxe.dll+00484164
[ 46] 0x000007febe4f745d bin\win64\pgo\m_lxe.dll+00488541
[ 47] 0x000007febe4f704f bin\win64\pgo\m_lxe.dll+00487503
[ 48] 0x000007febe600fb4 bin\win64\pgo\m_lxe.dll+01576884 MathWorks::lxe::StartupLxeEngine+00374224
[ 49] 0x000007febe4ff30b bin\win64\pgo\m_lxe.dll+00520971
[ 50] 0x000007febe4f562e bin\win64\pgo\m_lxe.dll+00480814
[ 51] 0x000007febe4f4358 bin\win64\pgo\m_lxe.dll+00475992
[ 52] 0x000007febe4f3fdc bin\win64\pgo\m_lxe.dll+00475100
[ 53] 0x000007fec1c625d0 bin\win64\pgo\m_dispatcher.dll+00075216 AutoPushingExecutionFrame::~AutoPushingExecutionFrame+00000784
[ 54] 0x000007fec1c6226d bin\win64\pgo\m_dispatcher.dll+00074349 Mfh_file::dispatch_with_reuse+00000045
[ 55] 0x000007febe50264c bin\win64\pgo\m_lxe.dll+00534092
[ 56] 0x000007febe50644b bin\win64\pgo\m_lxe.dll+00549963
[ 57] 0x000007febe506389 bin\win64\pgo\m_lxe.dll+00549769
[ 58] 0x000007fec16ac35b bin\win64\pgo\m_interpreter.dll+00050011 inFullFevalFcn+00000379
[ 59] 0x000007fec1c5b3bc bin\win64\pgo\m_dispatcher.dll+00046012 Mfh_MATLAB_fn_impl::dispatch_mf_with_reuse+00000172
[ 60] 0x000007fec1c61f12 bin\win64\pgo\m_dispatcher.dll+00073490 Mlm_file::needToCheckoutLicense+00002674
[ 61] 0x000007fec1c6143d bin\win64\pgo\m_dispatcher.dll+00070717 Mfh_MATLAB_fn_impl::dispatch+00000045
[ 62] 0x000007febe503898 bin\win64\pgo\m_lxe.dll+00538776
[ 63] 0x000007febe4cc386 bin\win64\pgo\m_lxe.dll+00312198
[ 64] 0x000007febe4cc270 bin\win64\pgo\m_lxe.dll+00311920
[ 65] 0x000007febe501ce4 bin\win64\pgo\m_lxe.dll+00531684
[ 66] 0x000007febe6189b1 bin\win64\pgo\m_lxe.dll+01673649 MathWorks::lxe::ShutdownLxeEngine+00081477
[ 67] 0x000007febe4f3f8d bin\win64\pgo\m_lxe.dll+00475021
[ 68] 0x000007febe4f6344 bin\win64\pgo\m_lxe.dll+00484164
[ 69] 0x000007febe4f745d bin\win64\pgo\m_lxe.dll+00488541
[ 70] 0x000007febe4f704f bin\win64\pgo\m_lxe.dll+00487503
[ 71] 0x000007febe600fb4 bin\win64\pgo\m_lxe.dll+01576884 MathWorks::lxe::StartupLxeEngine+00374224
[ 72] 0x000007febe4ff30b bin\win64\pgo\m_lxe.dll+00520971
[ 73] 0x000007febe4f562e bin\win64\pgo\m_lxe.dll+00480814
[ 74] 0x000007febe4f46ac bin\win64\pgo\m_lxe.dll+00476844
[ 75] 0x000007febe4b09aa bin\win64\pgo\m_lxe.dll+00199082
[ 76] 0x000007febe4b0793 bin\win64\pgo\m_lxe.dll+00198547
[ 77] 0x000007febe50644b bin\win64\pgo\m_lxe.dll+00549963
[ 78] 0x000007febe506389 bin\win64\pgo\m_lxe.dll+00549769
[ 79] 0x000007fec16ac35b bin\win64\pgo\m_interpreter.dll+00050011 inFullFevalFcn+00000379
[ 80] 0x000007fec1c5b3bc bin\win64\pgo\m_dispatcher.dll+00046012 Mfh_MATLAB_fn_impl::dispatch_mf_with_reuse+00000172
[ 81] 0x000007fec1c61f12 bin\win64\pgo\m_dispatcher.dll+00073490 Mlm_file::needToCheckoutLicense+00002674
[ 82] 0x000007fec1c6143d bin\win64\pgo\m_dispatcher.dll+00070717 Mfh_MATLAB_fn_impl::dispatch+00000045
[ 83] 0x000007febe503898 bin\win64\pgo\m_lxe.dll+00538776
[ 84] 0x000007febe4cc386 bin\win64\pgo\m_lxe.dll+00312198
[ 85] 0x000007febe4aeabf bin\win64\pgo\m_lxe.dll+00191167
[ 86] 0x000007febe501ce4 bin\win64\pgo\m_lxe.dll+00531684
[ 87] 0x000007febe63602d bin\win64\pgo\m_lxe.dll+01794093 mwboost::archive::detail::oserializer<mwboost::archive::binaryTerm_oarchive,ir::IrTree>::oserializer<mwboost::archive::binaryTerm_oarchive,ir::IrTree>+00039769
[ 88] 0x000007febe4f3f8d bin\win64\pgo\m_lxe.dll+00475021
[ 89] 0x000007febe4f6344 bin\win64\pgo\m_lxe.dll+00484164
[ 90] 0x000007febe4f745d bin\win64\pgo\m_lxe.dll+00488541
[ 91] 0x000007febe4f704f bin\win64\pgo\m_lxe.dll+00487503
[ 92] 0x000007febe600fb4 bin\win64\pgo\m_lxe.dll+01576884 MathWorks::lxe::StartupLxeEngine+00374224
[ 93] 0x000007febe4ff30b bin\win64\pgo\m_lxe.dll+00520971
[ 94] 0x000007febe4f562e bin\win64\pgo\m_lxe.dll+00480814
[ 95] 0x000007febe4f4358 bin\win64\pgo\m_lxe.dll+00475992
[ 96] 0x000007febe4f3fdc bin\win64\pgo\m_lxe.dll+00475100
[ 97] 0x000007fec1c625d0 bin\win64\pgo\m_dispatcher.dll+00075216 AutoPushingExecutionFrame::~AutoPushingExecutionFrame+00000784
[ 98] 0x000007fec1c6226d bin\win64\pgo\m_dispatcher.dll+00074349 Mfh_file::dispatch_with_reuse+00000045
[ 99] 0x000007fec00b6ae2 bin\win64\pgo\m_lxe.dll+29584098 mwboost::archive::detail::pointer_oserializer<mwboost::archive::binaryTerm_oarchive,MathWorks::lxe::MatlabIrTree>::save_object_ptr+00758386
[100] 0x000007febe50644b bin\win64\pgo\m_lxe.dll+00549963
[101] 0x000007febe506389 bin\win64\pgo\m_lxe.dll+00549769
[102] 0x000007fec16ac35b bin\win64\pgo\m_interpreter.dll+00050011 inFullFevalFcn+00000379
[103] 0x000007fec1c5b3bc bin\win64\pgo\m_dispatcher.dll+00046012 Mfh_MATLAB_fn_impl::dispatch_mf_with_reuse+00000172
[104] 0x000007fec1c61f12 bin\win64\pgo\m_dispatcher.dll+00073490 Mlm_file::needToCheckoutLicense+00002674
[105] 0x000007fec1c6143d bin\win64\pgo\m_dispatcher.dll+00070717 Mfh_MATLAB_fn_impl::dispatch+00000045
[106] 0x000007febe503898 bin\win64\pgo\m_lxe.dll+00538776
[107] 0x000007febe4cc386 bin\win64\pgo\m_lxe.dll+00312198
[108] 0x000007febe4aeb39 bin\win64\pgo\m_lxe.dll+00191289
[109] 0x000007febe501ce4 bin\win64\pgo\m_lxe.dll+00531684
[110] 0x000007febe63602d bin\win64\pgo\m_lxe.dll+01794093 mwboost::archive::detail::oserializer<mwboost::archive::binaryTerm_oarchive,ir::IrTree>::oserializer<mwboost::archive::binaryTerm_oarchive,ir::IrTree>+00039769
[111] 0x000007febe50033b bin\win64\pgo\m_lxe.dll+00525115
[112] 0x000007febe4fe6ff bin\win64\pgo\m_lxe.dll+00517887
[113] 0x000007febe4f562e bin\win64\pgo\m_lxe.dll+00480814
[114] 0x000007febe4f4358 bin\win64\pgo\m_lxe.dll+00475992
[115] 0x000007febe4f3fdc bin\win64\pgo\m_lxe.dll+00475100
[116] 0x000007fec1c625d0 bin\win64\pgo\m_dispatcher.dll+00075216 AutoPushingExecutionFrame::~AutoPushingExecutionFrame+00000784
[117] 0x000007fec1c6226d bin\win64\pgo\m_dispatcher.dll+00074349 Mfh_file::dispatch_with_reuse+00000045
[118] 0x000007febe50264c bin\win64\pgo\m_lxe.dll+00534092
[119] 0x000007febe50644b bin\win64\pgo\m_lxe.dll+00549963
[120] 0x000007febe506389 bin\win64\pgo\m_lxe.dll+00549769
[121] 0x000007fec16ac35b bin\win64\pgo\m_interpreter.dll+00050011 inFullFevalFcn+00000379
[122] 0x000007fec1c5b3bc bin\win64\pgo\m_dispatcher.dll+00046012 Mfh_MATLAB_fn_impl::dispatch_mf_with_reuse+00000172
[123] 0x000007fec1c61f12 bin\win64\pgo\m_dispatcher.dll+00073490 Mlm_file::needToCheckoutLicense+00002674
[124] 0x000007fec1c6143d bin\win64\pgo\m_dispatcher.dll+00070717 Mfh_MATLAB_fn_impl::dispatch+00000045
[125] 0x000007febe503898 bin\win64\pgo\m_lxe.dll+00538776
[126] 0x000007febe4cc386 bin\win64\pgo\m_lxe.dll+00312198
[127] 0x000007febe4aeb39 bin\win64\pgo\m_lxe.dll+00191289

 

0 Kudos
Reply

13,715 Views
adriantudor
NXP Employee
NXP Employee

Hi @nofake_drstrang ,

I hope that you have cleared the path and then set again to the new version of S12Z toolbox.

If you already have done that, please try to reboot your PC.

Best regards,

Adrian

0 Kudos
Reply

13,697 Views
nofake_drstrang
Contributor III

Hi @adriantudor ,

yes I did. But same crash...

Best regards

 

 

 

 

0 Kudos
Reply

13,690 Views
adriantudor
NXP Employee
NXP Employee

Hi @nofake_drstrang ,

 

 Can you give me the full path to "PMSM_ClosedLoop_Sensorless_S12ZVM.mdl", for default location?

 

Best regards,

Adrian

0 Kudos
Reply

13,687 Views
nofake_drstrang
Contributor III

@adriantudor 

yes, it is default location.

C:\Users\drstrange\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\BLDC_Demo\BLDC_ClosedLoop

 

and

 

C:\Users\drstrange\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop

0 Kudos
Reply

13,676 Views
paulvlase
NXP Employee
NXP Employee

Hi @nofake_drstrang ,

 

Can you try to install the latest Matlab R2020a update?

 

Here are the instruction to do that: https://www.mathworks.com/downloads/web_downloads/download_update?release=R2020a&s_tid=ebrg_R2020a_2...

 

Also you could try to change the location of the Matlab Add-Ons folder from Matlab Preferences -> MATLAB -> Add-Ons to something like C:\MatlabAddons\, reinstall the S12ZVM toolbox, and try again.

 

paulvlase_0-1599837559225.png

 

Regards,

Paul

0 Kudos
Reply

13,642 Views
nofake_drstrang
Contributor III

Hi @paulvlase ,

unfortunately it does not help with moving addon and reinstall the toolbox to C:\MatlabAddons\Toolboxes\NXP_MBDToolbox_S12ZVMx 

access_right.PNGcrash_newPath.PNG

Nice weekend!

 

0 Kudos
Reply

13,668 Views
nofake_drstrang
Contributor III

Hi @paulvlase

thanks for your reply!

 

Unfortunately we are not on Matlab Software Maintenance anymore. So we can not update matlab.

I recently tried the example model: C:\Freescale\MCToolbox\amclib\ammclib_amclib_observer_F16_s12zvm.mdl (I moved to C:\Freescale\MCToolbox; because of too long name issue)

Everything works fine, I can control and compare the results with Freemaster..

FreeMa_Obs.PNG

For me, it seems the model "PMSM_ClosedLoop_Sensorless_S12ZVM.mdl" has some problems.

But yes, I will try your suggestion with the reinstall of the toolbox to C:\MatlabAddons\

and I let you know..

 

Many thanks in advance!

0 Kudos
Reply