Recovery from LIN error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Recovery from LIN error

跳至解决方案
3,793 次查看
ruihang_wu
Contributor III

How should we use the toolbox to handle errors during LIN communication?

For example, if the slave is supposed to respond to the header when the frame ID is 1, and it doesn't respond for whatever reason, I'm seeing that the master kind of gets stuck and never sends out anything else, even if I try to send another header on the master.

Using freemaster I can see that the lin1_State.isBusBusy and lin1_State.isRxBusy are both set to true. I'm wondering how I could reset the state and try to send out another header if the slave does not respond to a master header.

0 项奖励
回复
1 解答
3,729 次查看
mariuslucianand
NXP Employee
NXP Employee
0 项奖励
回复
3 回复数
3,790 次查看
bryant48
Contributor I
0 项奖励
回复
3,776 次查看
ruihang_wu
Contributor III

Yes I have followed the examples outlined in that tutorial. It doesn't really explain how to handle bus errors.

0 项奖励
回复
3,730 次查看
mariuslucianand
NXP Employee
NXP Employee
0 项奖励
回复