Recovery from LIN error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recovery from LIN error

ソリューションへジャンプ
3,919件の閲覧回数
ruihang_wu
Contributor III

How should we use the toolbox to handle errors during LIN communication?

For example, if the slave is supposed to respond to the header when the frame ID is 1, and it doesn't respond for whatever reason, I'm seeing that the master kind of gets stuck and never sends out anything else, even if I try to send another header on the master.

Using freemaster I can see that the lin1_State.isBusBusy and lin1_State.isRxBusy are both set to true. I'm wondering how I could reset the state and try to send out another header if the slave does not respond to a master header.

0 件の賞賛
返信
1 解決策
3,855件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee
0 件の賞賛
返信
3 返答(返信)
3,916件の閲覧回数
bryant48
Contributor I
0 件の賞賛
返信
3,902件の閲覧回数
ruihang_wu
Contributor III

Yes I have followed the examples outlined in that tutorial. It doesn't really explain how to handle bus errors.

0 件の賞賛
返信
3,856件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee
0 件の賞賛
返信