Re: Pil Mode on KV3x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: Pil Mode on KV3x

1,774 Views
pbgemann001
Contributor III

Hi paulvlase,

another problem occured. After setting up on another PC everything except the PIL works. I get the following error

PILfail.PNG

I am using the same model, Matlabversion and DevBoard as before.

I will attach the slprj and the diagnostics output.

I guess it has to do with the location of files again? I have installed Matlab in D instead C on this PC could that be the cause?

Thank you for your help

Paul

0 Kudos
Reply
1 Reply

1,633 Views
paulvlase
NXP Employee
NXP Employee

Hi [email protected]‌,

Sorry for answering so late, but we were working on MBDT for S32K 4.0.1 release.

Right now the PIL is not working using the GCC compiler, somehow the application crashes on the board. I mentioned that here https://community.nxp.com/message/1145564#comment-1162694 .

I will try to fix this issue the next week.

Can you try to run PIL simulation using the IAR compiler?

0 Kudos
Reply