RGBLED mismatch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RGBLED mismatch

跳至解决方案
2,838 次查看
RegulusCheng
Contributor III

lHi,

I am using S32K3X4EVB-Q172 board with Simulink in Matlab 2021b.

MBDT Version 1.4.0

 

I try to use the Dio Example, in whitch the Red LED will flah and the Bule LED will open when push user buttom. 

I have successfully download the program. however, I found that the RGBLED never shine, instead, the Reset LED behaves as what RGBLED should behave: it flashed and keep open when I push user buttom. 

I have change the hardware to S32K344-Q172 in Model Configuration.

Please help me if you have suggestion.

RegulusCheng_0-1705309685507.pngRegulusCheng_1-1705309707113.png

 

RegulusCheng_4-1705309898046.png

 

 
0 项奖励
回复
1 解答
2,824 次查看
georgevictor
NXP Employee
NXP Employee

Hi, @RegulusCheng,

 

Thank you for using MBDT on your projects.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

 

Best regards,

Victor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,825 次查看
georgevictor
NXP Employee
NXP Employee

Hi, @RegulusCheng,

 

Thank you for using MBDT on your projects.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

 

Best regards,

Victor

0 项奖励
回复
2,809 次查看
RegulusCheng
Contributor III

Thank you, Victor

I change the Jumper31 as you said in that thread, and the board runs as wish.

I noticed that the reason of this problem is not found, if you found the final solution, please let me know

标记 (1)
0 项奖励
回复