RGBLED mismatch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,889件の閲覧回数
RegulusCheng
Contributor III

lHi,

I am using S32K3X4EVB-Q172 board with Simulink in Matlab 2021b.

MBDT Version 1.4.0

 

I try to use the Dio Example, in whitch the Red LED will flah and the Bule LED will open when push user buttom. 

I have successfully download the program. however, I found that the RGBLED never shine, instead, the Reset LED behaves as what RGBLED should behave: it flashed and keep open when I push user buttom. 

I have change the hardware to S32K344-Q172 in Model Configuration.

Please help me if you have suggestion.

RegulusCheng_0-1705309685507.pngRegulusCheng_1-1705309707113.png

 

RegulusCheng_4-1705309898046.png

 

 
0 件の賞賛
返信
1 解決策
2,875件の閲覧回数
georgevictor
NXP Employee
NXP Employee

Hi, @RegulusCheng,

 

Thank you for using MBDT on your projects.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

 

Best regards,

Victor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,876件の閲覧回数
georgevictor
NXP Employee
NXP Employee

Hi, @RegulusCheng,

 

Thank you for using MBDT on your projects.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

 

Best regards,

Victor

0 件の賞賛
返信
2,860件の閲覧回数
RegulusCheng
Contributor III

Thank you, Victor

I change the Jumper31 as you said in that thread, and the board runs as wish.

I noticed that the reason of this problem is not found, if you found the final solution, please let me know

タグ(1)
0 件の賞賛
返信