RGBLED mismatch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGBLED mismatch

Jump to solution
2,874 Views
RegulusCheng
Contributor III

lHi,

I am using S32K3X4EVB-Q172 board with Simulink in Matlab 2021b.

MBDT Version 1.4.0

 

I try to use the Dio Example, in whitch the Red LED will flah and the Bule LED will open when push user buttom. 

I have successfully download the program. however, I found that the RGBLED never shine, instead, the Reset LED behaves as what RGBLED should behave: it flashed and keep open when I push user buttom. 

I have change the hardware to S32K344-Q172 in Model Configuration.

Please help me if you have suggestion.

RegulusCheng_0-1705309685507.pngRegulusCheng_1-1705309707113.png

 

RegulusCheng_4-1705309898046.png

 

 
0 Kudos
Reply
1 Solution
2,860 Views
georgevictor
NXP Employee
NXP Employee

Hi, @RegulusCheng,

 

Thank you for using MBDT on your projects.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

 

Best regards,

Victor

View solution in original post

0 Kudos
Reply
2 Replies
2,861 Views
georgevictor
NXP Employee
NXP Employee

Hi, @RegulusCheng,

 

Thank you for using MBDT on your projects.

It looks like your evaluation board enters into a sequential reset state. Please review the following thread  S32K3X4EVB-T172 with MBD which addresses the same issue.

 

Best regards,

Victor

0 Kudos
Reply
2,845 Views
RegulusCheng
Contributor III

Thank you, Victor

I change the Jumper31 as you said in that thread, and the board runs as wish.

I noticed that the reason of this problem is not found, if you found the final solution, please let me know

Tags (1)
0 Kudos
Reply