Purpose of "Please restart Evaluation Board" message box?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Purpose of "Please restart Evaluation Board" message box?

跳至解决方案
3,611 次查看
rsating
Contributor III

Please help us understand the purpose of the message box that says "Please restart Evaluation Board to move processor to BAM mode and press OK", see attached screenshot.  This message box is displayed when we build code in the Matlab/Simulink MBDT examples. 

Is a reset sufficient?  Is it really necessary to power cycle the board?  And why?

Thanks

 

 

标签 (1)
0 项奖励
回复
1 解答
3,589 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating,

Thank you for your interest in our MBDT Toolbox!

The message that pops up, telling the user to reset the board, asks for a reset from the button, not necessarily power down and power up, in order to set the board in the bootloader. When the MCU boots up, it enters the bootloader (that has to be flashed previously using the S32DS according to the quick start guide). When the processors boot up, it enters bootloader and waits for a five seconds for a new firmware to be delivered over UART. If it receives nothing from the host computer, then the bootloader starts executing the code already stored in the flash memory.

So the mechanism is as follows:

1. Simulink generates and compiles the code, and shows that popup message.

2. The user resets the board and within 5 seconds press the 'OK' button.

3. If everything works fine, the host sends the new firmware to the board and the board boots the new code.

Hope this helps,

Marius

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,590 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating,

Thank you for your interest in our MBDT Toolbox!

The message that pops up, telling the user to reset the board, asks for a reset from the button, not necessarily power down and power up, in order to set the board in the bootloader. When the MCU boots up, it enters the bootloader (that has to be flashed previously using the S32DS according to the quick start guide). When the processors boot up, it enters bootloader and waits for a five seconds for a new firmware to be delivered over UART. If it receives nothing from the host computer, then the bootloader starts executing the code already stored in the flash memory.

So the mechanism is as follows:

1. Simulink generates and compiles the code, and shows that popup message.

2. The user resets the board and within 5 seconds press the 'OK' button.

3. If everything works fine, the host sends the new firmware to the board and the board boots the new code.

Hope this helps,

Marius

0 项奖励
回复
3,511 次查看
Lavern
Contributor I

Thanks for sharing this answer to us.

标记 (1)
0 项奖励
回复