Programming the internal flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming the internal flash

2,938件の閲覧回数
raghurajappa
Contributor IV

Using MPC5643L + Daughter board + Mother board XPC56xx EVB. 
Using Simulink + Green Hills v5.1.7 compiler + Serial interface.

Within Simulink I indicate the application to reside inside the internal Flash. I found out that there is NO .rbf file for MPC5643L. Hence using the .rba default file, I am programming using RappID. 

The problem - The application is NOT automatically started after reset/power off-on. How can I solve this? I understand that the bootloader and application needs to reside inside the internal Flash. But how can I achieve this using what is available?? What I understand is right now, the Bootloader is being programmed into the internal RAM and NOT internal Flash. This is the problem, as per my understanding. 

Please correct me and help me fix this problem? How can I make sure that my application is not "lost" after a power off! 

Thank you :smileyhappy: 

0 件の賞賛
返信
2 返答(返信)

2,730件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lazyJ ,

Can you help us with some insights in this matter?

As far as i know the BAM support only RAM download in case of the MPC5643L. Is that true ? 

Thank you!

Daniel

0 件の賞賛
返信

2,730件の閲覧回数
raghurajappa
Contributor IV

dumitru-daniel.popa, you're my savior :smileyhappy: 

0 件の賞賛
返信