Problems with PMSM model from Workshop Module M5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with PMSM model from Workshop Module M5

11,375件の閲覧回数
wangxuan
Contributor III

Hi,dumitru-daniel.popa

I made some further changes to the model modified by Leon Thürnau to make it work with KV4. I removed the Simulink Data Type Conversion module for multiplication. However, it has problems in the motor model. From the waveform point of view, the measured currents of phase A, phase B and phase C are correct. I do not know why the speed and back EMF of the motor are always zero, and I can not find the reason. I have attached my model. I hope you can help me, thank you!

17 返答(返信)

10,673件の閲覧回数
lethuer
Contributor V

Hello dumitru-daniel.popa

like you have shown in module 5 I want to measure the voltages directly with an oscilloscope:

Phase A &B terminal voltages and Line A-B resulting voltage.png

For me it was only possible to get this (Motor is not connected):

A - Terminal Phase A, GND

B - Terminal Phase B, GND

M - A-B (Math Operation)

Oszilloskopbild PWM_A PWM_B Line Voltage A-B 10 kHz.png

So the line voltage A-B does not have the same trend as yours.

Mine is only positive or negative because the PWM signals are centered and not shiftet like you signals.

It doesn't madder if I'm using the "eFlexPWM_Three_Phase_Output", three single "eFlexPWM_Complementary_Output" or the "FTM_Three_Phase_Output" block...

With Freemaster I could see this signals, which are fine.

Reference Voltages FreeMASTER.PNG

So it has to depend on the PWM block ? Are there any differences between S32K and KV4x ?

Best regards

Leon

0 件の賞賛
返信

10,673件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Leon, 

The commands looks OK. It seems like you are using Center Aligned PWM strategy while on S32K i used edge aligned PWM. 

For the KV4 toolbox you can select edge aligned only on Independent output block.

Anyhow that should not be an issue during the operation.

Best regards,

Daniel

0 件の賞賛
返信

10,673件の閲覧回数
lethuer
Contributor V

Hello dumitru-daniel.popa

I want to make my last post here, so you can find it better in the middle of all the other posts.

 

I'm now able to download the code to the target and checked the variables in freemaster (only in polling mode) like you did in module 5 !

The download works anytime successful but it only runs if the Driver Subsystem FNB41560 is commented out.

So the ADC communication makes anything wrong.

Do you see the mistake in the subsystem ?

Unbenannt.PNG

FNB41560:

Unbenannt1.PNG

ADC Samples:

Unbenannt2.PNG

 

Also this question is still relevant for me:

For example I want to stop the PWM if temperature is higher than 100°C.

By the way: What is your temperature recommendation for shutting down ?

 

Best regards and allways thank you for so much help ! You are a great teacher !

 

Leon

0 件の賞賛
返信

10,673件の閲覧回数
lethuer
Contributor V

Okay I solved the Problem by myself.

I remembered a few weeks ago and now I used priorities for the blocks to change the execution order.

ADC_Config (priority 1)

ADC StartA (priority 1)

ADC StartB (priority 1)

ADC Samples (priority 2)

I think the Problem was that the ADC Read block was executed before the ADC Start, Sample and Config blocks ?

This blocks always has to be executed before the ADC Read ?

So only this question is actual relevant:

For example I want to stop the PWM if temperature is higher than 100°C.

By the way: What is your temperature recommendation for shutting down ?

Best regards

Leon

10,673件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Leon, 

In general you do not stop the motor if the temperature exceeds a certain limit - you just throttle it down by reducing the current until the temperature decreases.

I'm not sure what temperature we are taking about there ? The temperature of the motor should be given by the manufacturer.

If you have a motor with neodymium PM than i would not go over 80 deg C.

Best regards,
Daniel

0 件の賞賛
返信

10,673件の閲覧回数
lethuer
Contributor V

Hello dumitru-daniel.popa

I think this is the temperature sensing to protect the 3-ph Driver ??

So I wanted to stop the PWM Generation directly to stop the current flow and avoid an overheating of the driver.

And I don't know the temperature limit of the Driver NXP has used for the HVP-MC3PH platform ?

Best regards

Leon

0 件の賞賛
返信

10,673件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Leon, 

I can't answer to that question since i have not found any references. Just play on the save side first and start with something like 65 deg C.

Alternatively you could search for the IGBT recommended temperature. 

Best regards,
Daniel

0 件の賞賛
返信

10,673件の閲覧回数
lethuer
Contributor V

Hi Daniel,

In the data sheet I found some information

http://www.mouser.com/ds/2/149/FNB41560-484544.pdf

Unbenannt.PNG

Unbenannt2.PNG

The "Total System" should be the complete Motion SPM FNB41560 Driver, so as absolut limit I would suggest 125°C.

Best regards

Leon

0 件の賞賛
返信

10,673件の閲覧回数
lethuer
Contributor V

Hi wangxuandumitru-daniel.popa

I'm now able to generate code for the embedded Hardware.

But during the build operation I got 6 warnings from the IAR Linker because of the blocks used in the Slow or Fast_Loop_Subsystem

Is that any Problem and how could I solve this ?

IAR ELF Linker V8.20.1.14183/W32 for ARM
   Copyright 2007-2017 IAR Systems AB.
Warning[Lt009]: Inconsistent wchar_t size
GFLIB_Cos.o(CM4_MMCLIB_IAR.a) and 4 other objects have wchar_t size
                      16 bits
            V_f_Scalar_Control_KV4x.o and 42 other objects, some of them in
                      dl7M_tln.a and 10 other libraries have wchar_t size 32
                      bits
Warning[Lt049]: Potential floating point parameter passing conflict. The first
          module below references the second and they have been built with
          different settings.
            AAPCS, VFP variant: V_f_Scalar_Control_KV4x.o
            AAPCS, base variant: GFLIB_Ramp.o(CM4_MMCLIB_IAR.a)
Warning[Lt049]: Potential floating point parameter passing conflict. The first
          module below references the second and they have been built with
          different settings.
            AAPCS, VFP variant: V_f_Scalar_Control_KV4x.o
            AAPCS, base variant: GFLIB_Sin.o(CM4_MMCLIB_IAR.a)
Warning[Lt049]: Potential floating point parameter passing conflict. The first
          module below references the second and they have been built with
          different settings.
            AAPCS, VFP variant: V_f_Scalar_Control_KV4x.o
            AAPCS, base variant: GFLIB_Cos.o(CM4_MMCLIB_IAR.a)
Warning[Lt049]: Potential floating point parameter passing conflict. The first
          module below references the second and they have been built with
          different settings.
            AAPCS, VFP variant: V_f_Scalar_Control_KV4x.o
            AAPCS, base variant: GMCLIB_ParkInv.o(CM4_MMCLIB_IAR.a)
Warning[Lt049]: Potential floating point parameter passing conflict. The first
          module below references the second and they have been built with
          different settings.
            AAPCS, VFP variant: V_f_Scalar_Control_KV4x.o
            AAPCS, base variant: GMCLIB_SvmStd.o(CM4_MMCLIB_IAR.a)
  13 794 bytes of readonly  code memory
     696 bytes of readonly  data memory
  14 573 bytes of readwrite data memory
Errors: none
Warnings: 6
Link time:   0.09 (CPU)   0.11 (elapsed)
Created executable: V_f_Scalar_Control_KV4x.elf

Best regards

Leon

0 件の賞賛
返信

10,673件の閲覧回数
lethuer
Contributor V

Hi wangxuan

good Job, we are getting closer ! Again I have attached my model.

I've seen your / mine / our modified model and think we could use the data type conversation in the Slow Loop Control Subsystem like shown below:

Unbenannt.PNG

Then the Speed_Reference (yellow line in COMMANDS) is exactly the same like in module 5 s32k example.

Your implemented gains in the Fast Loop Control Subsystem

Unbenannt3.PNG

 Now I was able to simulate correctly. Here are the results:

Unbenannt4.PNG

Unbenannt5.PNG

Like you see the COMMANDS and SVM are completely the same like in s32k module 5.

(U_Alpha and U_Beta are still upscaled)

But in EFFECTS we have some differences, the Motor Speed swings extremely:

Unbenannt6.PNG

I have made some Simulation runs (blue --> wc = 0.001; yellow --> wc = 1; red --> original pmsm module5)

Unbenannt8.PNG

How we could get the same result as in the pmsm Workshop module5 (red line) ?

After this step is done we could parametrize our own Motor with the values of R,L and so on.

Another way could be to use the Simscape Power Systems Toolbox instead of the Simulink PMSM model.

Also the Parameters of the LUT in the Slow Loop Control Subsystem I didn't have parametrized yet.

If this is done I want to download the code to the target and see the results in FreeMASTER.

Best regards

10,673件の閲覧回数
wangxuan
Contributor III

Hi Leon Thürnau,dumitru-daniel.popa

      Good job! I got the same result as yours,  I found that the back EMF we got was very large at the beginning, and the speed oscillations were obvious at this time. I think the problem lies in this (I do not know if I am correct), because rightly, our speed should be small at the outset, So the back-EMF should also be small, I think it should be caused by motor parameters do not match. The bus voltage we needed was 27 times larger, resulting in a large input phase voltage (about 150 times larger). I modified it according to the PMSM motor parameters in Table 1 and the current reached 300A (which seems to be wrong ), The following is the result I got. It seems that the speed oscillation problem appears to be getting better, but the phase current waveform changes greatly compared with the original one. In contrast, because the back EMF phase and the phase voltage phase are offset, Becomes no longer symmetrical. What do you think and correct? Thank you!

  

motor model

60ST-M01330

Rated power (W

400

Rated line voltage(V

220

Rated line current(A

2.8

Rated speed(rpm

3000

Rated torque(N.m

1.27

Peak torque(N.m

3.8

Back EMF(V/krpm

28

Torque coefficient(N.m/A

0.5

Rotor inertia(Kg.m2

0.302×10-4

Winding (Line) Resistance Ω

5.83

Winding (Line) Inductance  mH

12.23

Electrical time constant (ms

2.1

pastedImage_3.png

pastedImage_7.png

pastedImage_5.png

pastedImage_8.png

Best regards,

wang xuan

10,673件の閲覧回数
lethuer
Contributor V

Hi,

with Udc = 12V in FNB41560 Subsystem and wc = 1 in PMSM model I got the same results like in module5 example.

Unbenannt.PNG

So in General the Problem is the higher bus voltage and another Motor.

I will try to parametrize my Motor and see what happens.

Best regards

0 件の賞賛
返信

10,673件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Wang Xuan, 

I have 2 concerns about your results:

#1: Speed goes down in the beginning: possible culprit: friction constant B and/or J

#2: You have huge currents in the motor: possible culprit: R and/or KV

Best regards,
Daniel

0 件の賞賛
返信

10,673件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

I've looked a bit over the model. I think is an issue related with MATLAB solvers for diff. equations. It looks like you changed the simulation parameters. Mine is using:

pastedImage_2.png

pastedImage_1.png

Anyhow, you could try to modify the wc initial condition. 

pastedImage_3.png

You should be able to start see speed & back-emf. If you need further details about the motor - then you can check this one: Dynamic Simulation of Electrical Machines and Drive Systems Using MATLAB GUI | InTechOpen 

Hope it helps!

Daniel

10,673件の閲覧回数
lethuer
Contributor V

Hi dumitru-daniel.popa

I don't have your advanced Parameters in the second Screen:

Unbenannt.PNG

How could I activate them ?

0 件の賞賛
返信

10,673件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Leon, 

That depends on MATLAB version you are using. Using an older version might not show them at all. Anyhow - i noticed that some of the parameters can only be found in the "All Parameters" Tab. Try to search it there.

Best regards,

Daniel

0 件の賞賛
返信

10,672件の閲覧回数
lethuer
Contributor V

Hi Daniel,

no I'm sorry..

Also in the "All Parameters" tab there are only the Options for "Signals", "Parameters" and "Data Store Memory block" but not your "Advanced Parameters".

Best regards

Leon

0 件の賞賛
返信