Problem with the configuration and operation of eMios Channels.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with the configuration and operation of eMios Channels.

1,572 次查看
Alfredo_Rubio
Contributor II

I'm working in Setting the base development environment for a DC/DC power converter.

This converter will be based on a interleave topology and them we need to control 3 half bridges basically working at 120º phase shift.

I’m using 1.4.0 MBD toolbox version with the R2022B matlab release.

I’m also using the NXP Configuration tool instead of the Tresos one.

As we need to keep in control the Phase shift we would like to work with the eMios channels configured in the OPWMCB mode. The idea is to implement the following scheme.

Alfredo_Rubio_0-1697442829332.png

 

I started from one of your sample projects (S32K344_pwm_center_aligned_ebt) modifying it and its configuration in order to adapt it to our requirements.

I this process I’m facing two different problems.

  1. LCU configuration:  I think that I configured it in the correct way, but after calling the MC_SetLcuSyncOutputEnable function no signal is present at the configured output pins. I have check the TRGMUX configuration redirecting its outputs to I/O pins and in this case, everything seems to be working properly.
  2. The second problem arise with the PWM_SetDutyCycle function.  I’ trying to update de Duty with the following scheme (copy form the example).

Alfredo_Rubio_1-1697442829337.png

 

The problem is that for the first of the channels updated, the Duty Cycle is no updated and its output is frozen to its default value (The one configured in the config tool). This happens always with the first channel that is written in the model. As you can see, I first wrote to the channel 1 and detect the problem in this channel. Then I configure a 4th channel to see is there was a problem with the number of configured channels, and everything works in the same way (channel 1 frozen to its default value and the three other channels changing its DutyCycle). The last test was to comment the write to the first channel. In this scenario, the problem appears on the second channel instead of the first one.

 

Could you give some clue on these problems?

0 项奖励
回复
3 回复数

1,545 次查看
Alfredo_Rubio
Contributor II

I solved the first problem.

It was my fault as I hadn't configured the LCU input multiplexer in the right way.

The second problem is still there. The first pwm eMios channel is hook to its default value despite the generate code is writing to it the new value.

Now I will procced to export the code to DS and procced to debug it.

0 项奖励
回复

1,391 次查看
RegulusCheng
Contributor III

Hello,

I have met the same problem with your first problem. Could you explain in some detail about your fault? What's wrong with your configuration exactly?

0 项奖励
回复

1,355 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hello @RegulusCheng 

First, I would recommend you to start by checking our s32k344_pwm_trgmux_lcu_adc_ctu_ebt example which can be found in the following path: <toolbox_root>/S32K3_Examples/pwm\s32k344_pwm_trgmux_lcu_adc_ctu_ebt.

The application demonstrates how LCU is configured to output 3 phases based on EMIOS signals sent via TRGMUX, and I think it would be a good starting point for investigating your problem, as the model and its associated configuration project, provide the necessary information on what functions should be called inside the application, and what are the required components configurations for enabling the LCU outputs.

In case this application does not provide the necessary information, please let us know more details on your use case so we could provide further guidance.

Thanks,

Irina

 

0 项奖励
回复