Problem with Block Config_Information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Block Config_Information

1,658件の閲覧回数
lukasschäfer
Contributor III

Hi,

i have sometimes a problem with the Config_Information Block:

188870_188870.pngConfig_Block.png

 

After a lot of compiling and flashing the device, there is a problem.

The diagnostic viewer says: Build error (see diagnostic.txt)

 

When i delete the Config_Information Block and put in a new Config Block, it works.

Thank you for help.

 

Best regards

Lukas

Original Attachment has been moved to: diagnostic.txt.zip

0 件の賞賛
返信
1 返信

1,542件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi lukasschäfer‌,

I've not met this kind of situation in before. 

Next time when this happens - can you delete the *_rtw automatic generated folder instead ?

I've a feeling that the root cause might be there instead of Simulink config block.

Keep us in the loop, and eventually try to send us the model when that issue occurs in order to try it on our side, hopefully to reproduce the error.

Thank you!

Daniel

0 件の賞賛
返信