Problem to connect to DEVKIT-MPC5744P with FreeMaster

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem to connect to DEVKIT-MPC5744P with FreeMaster

ソリューションへジャンプ
3,471件の閲覧回数
alexandreboyer
Contributor I

Dear Dimitri,

thank you for this very interesting tutorial. I succeed in installing Model Based Design Toolbox and programming MPC5744P development kit with Simulink. However, I have a problem with Freemaster 2.0 when I try to connect to DEVKIT-MPC5744P.

The message below arises:

pastedImage_1.png

Even if I load no source file and I try only to connect to the board, when I click to Start/stop communications, this error message arises.

Could you help me to solve this problem ?

Alexandre

0 件の賞賛
返信
1 解決策
3,156件の閲覧回数
alexandreboyer
Contributor I

I had brought the solutions suggested in the different Hotfixes. Everything works after a simple restart of my computer. So, now everythink works fine.

元の投稿で解決策を見る

2 返答(返信)
3,157件の閲覧回数
alexandreboyer
Contributor I

I had brought the solutions suggested in the different Hotfixes. Everything works after a simple restart of my computer. So, now everythink works fine.

3,156件の閲覧回数
jimduanva
Contributor II

I have the same problem.

My tools:  Matlab is 2016a;@ NXP MBDT is 2.0; S32 Design Studio is 2017 R1 with updates

Build and Download are ok, not able to connect to FreeMaster.

Tried the Hotfix3 in https://community.nxp.com/thread/451804. No luck on it.

Tried the solution of https://community.nxp.com/thread/454868. The FreeMaster works by using RAppID.exe to flash the bin file ADC1.mot under Daniel's comment.

Please Help.

Thanks,

JD

0 件の賞賛
返信