One interupt multiple SM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

One interupt multiple SM

1,133件の閲覧回数
JustMet
Contributor III

Hello all,
I am trying to create a SENT tx block which uses FlexIO, my idea is for a user to drag and drop the box and then in the box select timer and shifter, and output pin wrt to selected timer and shifter, for example, FLEXIOD2/3 are mapped to shifter1 and timer1 respectively and since there are multiple NXP pin associated to D3 pin with different mux I want the user to select this pin.


But the problem I get is in parameter passing, and I can only have one instance of flexio interrupt so is there any way possible that interrupt is defined once, and then all the other blocks work as SM inside the interrupt.

Best regards,
JustMet

0 件の賞賛
返信
0 返答(返信)