Model Reference using function calls in NxP_MPC57x Toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model Reference using function calls in NxP_MPC57x Toolbox

1,477 Views
QuentinBEGON
Contributor I

Dear MBD Team,

I am using NXP_MBDToolbox_MPC57xx(v 3.2.0).

I am trying to simulate via the PIL mode but I am not able to use a reference model using function calls with this toolbox.

I get an error : the MBD_MPC574x_Config_Information block is a non-virtual block and it cannot be placed in an export-function model unless it has a constant sample time.

I tried to put the MBD_MPC574x_Config_Information block only in the top model but with a reference model, it is mandatory to put one inside. 

Here my questions :

1. Is it possible to use MODEL Referencing with function calls and this toolbox?

2. If yes, how?

Please find attached example and the error. 

Thank you for your time and your help.

Best Regards,

Quentin BEGON

0 Kudos
Reply
0 Replies