NXP_MBDToolbox_IMXRT1xxx example running problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP_MBDToolbox_IMXRT1xxx example running problem

ソリューションへジャンプ
2,422件の閲覧回数
Paul_Kang
NXP Employee
NXP Employee

Hello,

 

I am trying to install MBDT for i.MXRT. I downloaded tool kit version 1.2.0 and I installed it with matlab 2020b. 

Based on description in quick start guide, I installed the tool and tried to run example. 

https://www.nxp.com/docs/en/quick-reference-guide/MBDT-IMXRT-QSG.pdf

As is described in 2.3 A “Hello World” Example, I tried to run GPIO interrupt example but as soon as I open "evkmimxrt1060_gpio_interrupt.mdl", I met below failure message. 

Could you help how I can fix this problem? 

Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handlers_list(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handler_properties(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_peripherals_list(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handlers_list(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handler_properties(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handler_properties(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handler_properties(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_peripherals_list(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handlers_list(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handler_properties(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".
Failure in datetime.datetime(647) : Could not recognize the date/time format of '23-4-2021 05:37:29'. You can specify a format using the 'InputFormat' parameter. If the date/time text contains day, month, or time zone names in a language foreign to the 'ko_KR' locale, those might not be recognized. You can specify a different locale using the 'Locale' parameter.
Failure in mbd_imxrt_isr_get_handler_properties(0) : Output argument "isrStruct" (and maybe others) not assigned during call to "mbd_imxrt_isr_get_xml_settings".

 

 

Best regards,

Paul

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,406件の閲覧回数
nxa11767
NXP Employee
NXP Employee

Hello Paul,

See this post for a fix to this datetime issue. When you run the mbdt_imxrt_path.m script did you see similar errors? The problem here is that the matlab date format must be consistent with your system settings for the datetime function to pass. Check also this post for v1.2.0 installation.

 

Best regards,

Alexandra 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,407件の閲覧回数
nxa11767
NXP Employee
NXP Employee

Hello Paul,

See this post for a fix to this datetime issue. When you run the mbdt_imxrt_path.m script did you see similar errors? The problem here is that the matlab date format must be consistent with your system settings for the datetime function to pass. Check also this post for v1.2.0 installation.

 

Best regards,

Alexandra 

0 件の賞賛
返信