NXP MBDT for S32K1x in MacOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP MBDT for S32K1x in MacOS

358 次查看
Yashwinder
Contributor I

Hello all, 

I installed the NXP MBDT Toolbox V 4.3.0 in Matlab R2025a in MacBook.

In the Library Browser, I am able to see the NXP toolboxes and can use to prepare the model. However I'm unable to run the model and facing this error.

"Error:Error evaluating 'InitFcn' callback of block_diagram 'Experiment_1_Model'.
Callback string is '
mbd_s32k_consistency_checks(bdroot(gcs));'
Caused by:
Index exceeds array bounds.

I even generated the license.dat file from NXP website but not sure if it's working. 

Can anyone suggest what can be done here?

 

@nxp MBDT 

标记 (4)
0 项奖励
回复
1 回复

289 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @Yashwinder 

Unfortunately, the MBDT provides support only for Windows operating systems, while Mac OS and Linux are not supported.

Regards,

Marius

0 项奖励
回复