NXP MBDT code import

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MBDT code import

1,632 Views
saurabhkulkarni123
Contributor II

Hello NXP

We are trying to import nxp mbdt generated code in to S32 IDE for ARM, through ProjectInfo.XML file but whenever we import the code, build option get disabled from the menu and we are not able to build it. 

Please give us a reply, Its urgent basis

0 Kudos
Reply
1 Reply

1,618 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hi @saurabhkulkarni123 ,

Perhaps the solution from this post could be of help in your use case as well. (https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-export-S32K144-MBDT-Generated-Co...)

Could you please check if the Model-Based Design Toolbox is installed in a path that contains spaces? In this case, please consider following the steps mentioned in the post attached for re-installing the toolbox in a path which does not contain spaces. 

Hope this helps,

Irina

0 Kudos
Reply