NXP MBDT S32k144 - PIL Eroor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MBDT S32k144 - PIL Eroor

2,298 Views
Shankar_Ancit
Contributor I

Hello

I'm trying to perform PIL (Processor-In-the-Loop) simulation from MATLAB Simulink. The RAppID Bootloader (RAppID BL) process completes successfully, but after that, I encounter the following error in Simulink:

Error:

An error occurred during simulation and the simulation was terminated. Caused by: The timeout of 10 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this communication failure. You should: (a) Check that the target hardware configuration is correct, for example, check that the byte ordering is correct. (b) Confirm that the target application is running on the target hardware. (c) Consider the possibility of application run-time failures (e.g. divide by zero exceptions, incorrect custom code integration, etc.). Note (c): To identify possible reasons for the run-time failure, consider using SIL, which supports signal handlers and debugging. If you cannot find a solution, consider using the method setTimeoutRecvSecs of rtw.connectivity.RtIOStreamHostCommunicator to increase the timeout value.
 
I am not getting the proper output from my PIL simulation. Can anyone assist me in resolving this issue? (Check the attached Screenshots below) Thank you.
0 Kudos
Reply
0 Replies