Mutiple ADCs data reading flucating badly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mutiple ADCs data reading flucating badly

812件の閲覧回数
noobsplzwin
Contributor III

Hello NXP Community,

I am working with an S32K344-based custom PCB and experiencing some issues with ADC readings. I have configured three ADC channels (ADC1(ADC0_P4), ADC2(ADC0_P3), and ADC3(ADC0_P0)) under ADC0Group1. For testing purposes, all three channels are connected to the same voltage source. I intended to compare the consistency of the readings across multiple ADC channels.

However, I am encountering an issue where only ADC1 provides stable data readings, while ADC2 and ADC3 show significant fluctuations despite being configured identically and sampling the same voltage source. I have attached relevant screenshots from FreeMASTER showing the fluctuating readings and my Simulink configuration showing the setup.

I also tried adding more channels to ADC0Group1. Every ADC after ADC1 fluctuates a lot.

noobsplzwin_1-1720202669455.pngnoobsplzwin_1-1720202669455.png

 

Attachments:

  1. FreeMASTER output showing the readings
  2. S32CT configuration of the ADC setup
  3. Simulink File

noobsplzwin_2-1720202785247.pngnoobsplzwin_2-1720202785247.png

noobsplzwin_3-1720202801583.pngnoobsplzwin_3-1720202801583.pngnoobsplzwin_4-1720202813819.pngnoobsplzwin_4-1720202813819.png

noobsplzwin_5-1720202823842.pngnoobsplzwin_5-1720202823842.png


I am wondering if there is something I am missing in the configuration or if there might be a known issue with such a setup. Any advice or suggestions would be greatly appreciated!

Thank you!
Connor

0 件の賞賛
返信
0 返答(返信)