Motor control toolbox for Kinetis V Series V1.40 missing repository information?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor control toolbox for Kinetis V Series V1.40 missing repository information?

Jump to solution
4,534 Views
liuqimin
Contributor IV

Hello:

When I open a KV mcu model in Simulink, a "Some libraries are missing repository information" error appearing. almost all the blocks in Motor control toolbox for Kinetis V Series are missing.and i must press the knob "fix" to reload this blocks.  what's the matter happened? this is a another bug?

OS WIN10 X64
IAR 8
MATLAB2017B

Best regards!

Liu qimin

Labels (1)
0 Kudos
Reply
1 Solution
4,321 Views
liuqimin
Contributor IV

Hi:

   After do the fix following  the instruction,this error message not show again.

 Thanks!

Liu qimin

View solution in original post

2 Replies
4,322 Views
liuqimin
Contributor IV

Hi:

   After do the fix following  the instruction,this error message not show again.

 Thanks!

Liu qimin

4,321 Views
Daniel_Popa
NXP Employee
NXP Employee
0 Kudos
Reply