Motor control toolbox for Kinetis V Series V1.40 missing repository information?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Motor control toolbox for Kinetis V Series V1.40 missing repository information?

ソリューションへジャンプ
4,498件の閲覧回数
liuqimin
Contributor IV

Hello:

When I open a KV mcu model in Simulink, a "Some libraries are missing repository information" error appearing. almost all the blocks in Motor control toolbox for Kinetis V Series are missing.and i must press the knob "fix" to reload this blocks.  what's the matter happened? this is a another bug?

OS WIN10 X64
IAR 8
MATLAB2017B

Best regards!

Liu qimin

ラベル(1)
0 件の賞賛
返信
1 解決策
4,285件の閲覧回数
liuqimin
Contributor IV

Hi:

   After do the fix following  the instruction,this error message not show again.

 Thanks!

Liu qimin

元の投稿で解決策を見る

2 返答(返信)
4,286件の閲覧回数
liuqimin
Contributor IV

Hi:

   After do the fix following  the instruction,this error message not show again.

 Thanks!

Liu qimin

4,285件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee
0 件の賞賛
返信