Motor Control Class: Lecture 1 - Introduction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor Control Class: Lecture 1 - Introduction

52,628 Views
Daniel_Popa
NXP Employee
NXP Employee

We start this course with this introduction video that present the hardware we will work with throughout this series. 

Main topics:

    - MPC5744P DevKit main hardware features;

    - MotorGD DevKit main hardware features;

    - How to install the Model Based Design Toolbox for MPC5744P revision 2.0.0;

    - How to generate a license;

    - How to setup a compiler toolchain using S32 Design Studio for Power Architecture;

    - How to add the Model Based Design Toolbox for MPC5744P into the Simulink Standard Libraries;

    - How to validate the software installation by generation C code for the first time;

Objectives:

    - Understand the hardware setup;

    - Download and Install the Model Based Design Toolbox for MPC5744P;

    - Generate a license for the toolbox;

    - Configure the toolbox and generate code for the first time;

Watch the introduction video and leave your comments and questions below.

(view in My Videos)

Additional information:

    - Model Based Design Toolbox for MPC5744P Installer: here

    - MPC5744P DevKit – Product Home Page: here

    - MotorGD DevKit – Product Home Page: here

    - MPC5744P DevKit – Quick Start Guide: here 

    - MPC5744P – Product Home Page: here

    - MPC5744P – Reference Manual: here

    - MPC5744P – Fact Sheet: here

    - MPC5744P – Data Sheet: here

    - MC34GD3000 – Data Sheet: here

    - BUK7K52-60E – Data Sheet: here

    - S32DS for PA (e200 core) – Download Link: here

    - PDF attached with main peripherals that we are going to use for motor control

NOTE: Chinese viewers can watch the video on YOUKU using this link.

注意:中国观众可以使用此链接观看YOUKU上的视频

33 Replies

22,692 Views
dsytj88
Contributor II

Daniel

sorry,even there is one button for download by your provided link,after clicking download button,

the file could be only saved as text format and finally downloading is failed.

if the file can be downloaded,then everything will be fine.

Best regards

david

0 Kudos
Reply

22,636 Views
Daniel_Popa
NXP Employee
NXP Employee

David, 

It might be something specific to your PC setup. We checked with other PCs from intranet and extranet and the site works OK. Also, i checked the logs and looks like other peoples can see it. Could it be something from your internet service provider ? 

Best regards,

Daniel

0 Kudos
Reply

22,515 Views
elite_lee
Contributor I

Daniel,

I can't see the video too.  The situation likes David :smileycry:. could you offer a link that i can download the video, because i can download the class's attachmet like the PDF.

捕获.PNG

0 Kudos
Reply

22,503 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Sun et .all with video issues, 

Can you try this link please: https://community.nxp.com/download-video!execute.jspa?videoID=7692 

You should see this page that allows you to download the video and see it offline.

Capture.JPG

If the issue will persists we will consider moving the video to YOUTUBE

Thanks for your understanding!

Best regards,
Daniel

0 Kudos
Reply

22,408 Views
paul_xu
Contributor II

Hi Daniel,

        I tried all the download link you have provided. It seems doesn`t work. As you know we can`t see the video on the YouTube without VPN, So it`s not convenient in China.

        If there is a way to share more related training data for download like PPT, so we can join the class in this way.

        QQ截图20170518091914.jpg

       Thanks for your support!

       Paul Xu

0 Kudos
Reply

12,591 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Paul, 

Thanks for your feedback. For the next videos i'm going to add more power point slides and will make them available for download. 

Anyhow, at the end of the series a full PDF will all the slides will become available as well.

Best regards,

Daniel

0 Kudos
Reply

7,829 Views
bruceye
Contributor II

Hi Daniel,

It is okay to download the video from your link but really slowly ,it seems that it will take me more than 10 hours.

Best regards
Bruce

0 Kudos
Reply

7,829 Views
bruceye
Contributor II

Hello ,

Somehow I cannot watch this video , does anyone has the same problem as I do ? Do I need to use some particular browsers?

Thank you 

Bruce

0 Kudos
Reply

7,829 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi lezhou ye, 

I'm sorry to hear that. It works fine with Chrome and IE. What kind of browser are you using?

Best regards,
Daniel

0 Kudos
Reply

7,829 Views
robin林
Contributor I

Hi dumitru-daniel.popa,

   You series of tutorials have documentation more than just video?Just like the MPC5744P data sheet 

    Best regards,
   Robin

0 Kudos
Reply

7,829 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Robin, 

Each section has the PDF document and Simulink Models (whenever is the case). Apart of that, we are using only NXP official documentation that could be found on the MPC5744P Documentation Official Page: MPC574xP|32-bit MCU|Chassis-Safety|NXP 

Let me know if there is something in particular about this processor that you look for and can't be found on the www.nxp.com

Thank you!

Daniel

0 Kudos
Reply

7,829 Views
bruceye
Contributor II

HI Daniel ,

I tried Chrome and IE but with no help .The screen turned out to be like this :

C@J1VK7}YH@{384FZEMGI9G.png

Thank you for your reply.

Bruce

0 Kudos
Reply

7,829 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Bruce,

Can you try with this link:  Video Link : 7692 

Just in case it does not work, you have the option to download the video and watch it offline with any video viewer.

Capture.JPG

Hope this will resolver your issue.

Best regards,
Daniel

0 Kudos
Reply