Module 5: V/F Scalar Control

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Module 5: V/F Scalar Control

956 次查看
AjRj14
Contributor III

Hi

I was simulating the simulink file of V/F scalar control(M5_2018.R1) which is available in https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Module-7-Torque-Control/m-p/736921.

When I gave 200 rad/sec as the commanded speed and simulated, the motor phase current is around 6 A (approx) , where as the load torque is zero.

As per the data sheet of Linix motor 45ZWN24-40, the max current is 2.3 A.

Could you please check and confirm the above query?

Thanks in advance.

 

AjRj14_0-1614947612168.pngAjRj14_0-1614947612168.png

 

 

0 项奖励
回复
0 回复数