Module 5: V/F Scalar Control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Module 5: V/F Scalar Control

950件の閲覧回数
AjRj14
Contributor III

Hi

I was simulating the simulink file of V/F scalar control(M5_2018.R1) which is available in https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Module-7-Torque-Control/m-p/736921.

When I gave 200 rad/sec as the commanded speed and simulated, the motor phase current is around 6 A (approx) , where as the load torque is zero.

As per the data sheet of Linix motor 45ZWN24-40, the max current is 2.3 A.

Could you please check and confirm the above query?

Thanks in advance.

 

AjRj14_0-1614947612168.pngAjRj14_0-1614947612168.png

 

 

0 件の賞賛
返信
0 返答(返信)