Model based CTU compile issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model based CTU compile issue

Jump to solution
2,981 Views
leeewayyy
Contributor II

Hi,

I have a issue when compiling the model based code:


Error: File: C:\Users\leewe\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx\mbdtbx_mpc574x\mbdtbx_mpc574x\blocks\ctu\ctu_mpc574x_config.tlc Line: 130 Column: 34
Unable to find pins within the user_config scope

Can anyone help me with that?

The model is attached below.

Regards,

Lee

1 Solution
2,876 Views
mariuslucianand
NXP Employee
NXP Employee

Hello leeewayyy‌,

Thank you very much for noticing this behaviour. I was able to replicate this and indeed is very strange.

However, I have updated the mbd_mpc574x_ec_toolbox.mdl file, that I was also attached to this response, so please backup the mbd_mpc574x_ec_toolbox.mdl file and then replace it with the one attached.

The file is located under [Toolbox Install Path]\mbdtbx_mpc574x\mbdtbx_mpc574x file.

Hope this helps,

Marius

View solution in original post

0 Kudos
Reply
3 Replies
2,877 Views
mariuslucianand
NXP Employee
NXP Employee

Hello leeewayyy‌,

Thank you very much for noticing this behaviour. I was able to replicate this and indeed is very strange.

However, I have updated the mbd_mpc574x_ec_toolbox.mdl file, that I was also attached to this response, so please backup the mbd_mpc574x_ec_toolbox.mdl file and then replace it with the one attached.

The file is located under [Toolbox Install Path]\mbdtbx_mpc574x\mbdtbx_mpc574x file.

Hope this helps,

Marius

0 Kudos
Reply
2,876 Views
leeewayyy
Contributor II

Hi mariuslucianandrei‌,

This works for me, thanks very much!

Regards,

Li

2,876 Views
leeewayyy
Contributor II

This only happens when i use CTU1 instead of CTU0.

0 Kudos
Reply