Model based CTU compile issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Model based CTU compile issue

ソリューションへジャンプ
3,201件の閲覧回数
leeewayyy
Contributor II

Hi,

I have a issue when compiling the model based code:


Error: File: C:\Users\leewe\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx\mbdtbx_mpc574x\mbdtbx_mpc574x\blocks\ctu\ctu_mpc574x_config.tlc Line: 130 Column: 34
Unable to find pins within the user_config scope

Can anyone help me with that?

The model is attached below.

Regards,

Lee

1 解決策
3,096件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello leeewayyy‌,

Thank you very much for noticing this behaviour. I was able to replicate this and indeed is very strange.

However, I have updated the mbd_mpc574x_ec_toolbox.mdl file, that I was also attached to this response, so please backup the mbd_mpc574x_ec_toolbox.mdl file and then replace it with the one attached.

The file is located under [Toolbox Install Path]\mbdtbx_mpc574x\mbdtbx_mpc574x file.

Hope this helps,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,097件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello leeewayyy‌,

Thank you very much for noticing this behaviour. I was able to replicate this and indeed is very strange.

However, I have updated the mbd_mpc574x_ec_toolbox.mdl file, that I was also attached to this response, so please backup the mbd_mpc574x_ec_toolbox.mdl file and then replace it with the one attached.

The file is located under [Toolbox Install Path]\mbdtbx_mpc574x\mbdtbx_mpc574x file.

Hope this helps,

Marius

0 件の賞賛
返信
3,096件の閲覧回数
leeewayyy
Contributor II

Hi mariuslucianandrei‌,

This works for me, thanks very much!

Regards,

Li

3,096件の閲覧回数
leeewayyy
Contributor II

This only happens when i use CTU1 instead of CTU0.

0 件の賞賛
返信