Model-Based Design Toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model-Based Design Toolbox

2,197 Views
zhouwenxiang
Contributor I
嘿,伙计们:

当我使用恩智浦的MBDT时,我不仅可以使用其中的模块在Simulink中进行仿真,还可以生成S32K的代码,因为我看到MBDT安装目录中有三个库文件。使用 Simulink 进行仿真时调用的库是否与生成嵌入式代码时调用的库不同?

谢谢lib_for_mbdt.jpg

0 Kudos
Reply
2 Replies

2,166 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

The NXP community is about helping each other and that's why it is English only, so other users can find solution to their problems as well. If possible, can you translate the question in English?

Best regards,

Bancila Sorin

0 Kudos
Reply

2,153 Views
zhouwenxiang
Contributor I

Dear NXP‘s team:

When I use NXP's MBDT, I can not only use its modules for simulation in Simulink, but also can generate code for S32K, then I see three library files in the MBDT installation directory.  It bothers me that is the library called when using Simulink for simulation different from the static library called when generating embedded code. Thanks

lib_for_mbdt.jpg

0 Kudos
Reply