Hi,
I have updated MBDT S32k3xx toolbox from 1.4 to 1.5 . After the update, deployment to the chip still go through the downloading process, however, the chip does not response. Let me know if there is an issue with setting in the configure tool or other problem that I have not resolve, thanks!
I have used the shared project from the community, it works great in 1.4 but encounter issue when updated to 1.5. The file is called Article 4 - MR-CANHUBK344_CAN.zip, which you can find in the link below.
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...