Model-Based Design Toolbox for S32K3xx 1.5.0 Deploy Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model-Based Design Toolbox for S32K3xx 1.5.0 Deploy Issue

972 Views
Wei_H
Contributor III

Hi,

I have updated MBDT S32k3xx toolbox from 1.4 to 1.5 . After the update, deployment to the chip still go through the downloading process, however, the chip does not response. Let me know if there is an issue with setting in the configure tool or other problem that I have not resolve, thanks!

I have used the shared project from the community, it works great in 1.4 but encounter issue when updated to 1.5. The file is called Article 4 - MR-CANHUBK344_CAN.zip, which you can find in the link below.

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

Tags (3)
0 Kudos
Reply
0 Replies