Model Based Design Toolbox License Missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Model Based Design Toolbox License Missing

5,403件の閲覧回数
jackjack
Contributor III

2018-04-06_210721.png

the hostID is right. I allready get the license, why would that error keeps coming up?

MPC5744P+matlab2016a+s32ds2017

5 返答(返信)

4,806件の閲覧回数
jackjack
Contributor III

i already tried this, but it doesn't work. maybe it has something to do with my driver.  i have a 128G SSD(driver C) + 500G HDD(driver D E F). matlab  and mbdt are both installed in driver D.

0 件の賞賛
返信

4,806件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Jack, 

What is the disk serial number of the partition used for MBDT installation (in fact how many numbers does it contains)?

Best regards,
Daniel

0 件の賞賛
返信

4,806件の閲覧回数
jackjack
Contributor III

I tried to install matlab, s32ds, mbdt for mpc5744p today,  the license error didn't show up,  but something else came up ,i am not sure what that means.this is the code generation diagnosic.

"系统找不到指定的路径 (The system can not find the specified path.)" 

### Generating code into build folder: D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw
### Invoking Target Language Compiler on adc_ctu_dma_model.rtw
### Using System Target File: D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tlc
### Loading TLC function libraries
### Initial pass through model to cache user defined code
### Caching model source code
### Writing source file adc_ctu_dma_model.c
### Writing header file adc_ctu_dma_model_private.h
### Writing header file adc_ctu_dma_model.h
### Writing header file adc_ctu_dma_model_types.h
### Writing header file rtwtypes.h
.
### Writing source file mbd_main.c
### Writing source file intc_sw_vectable.c
### Writing source file intc_init.c
### Writing header file bam_defines.h
### Writing header file target.h
### TLC code generation complete.
### Creating project marker file: rtw_proj.tmw
.### Evaluating PostCodeGenCommand specified in the model
.
### Processing Template Makefile: D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tmf
### Creating adc_ctu_dma_model.mk from D:\Program Files\MBDToolbox\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\mbd_pnt.tmf
### Building adc_ctu_dma_model: .\adc_ctu_dma_model.bat

D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw>set MATLAB=D:\Program Files\Matlab2016a

D:\matlab_vcu\adc_ctu_dma_model_mbd_rtw>"D:\Program Files\Matlab2016a\bin\win64\gmake" -f adc_ctu_dma_model.mk COPY_MDLREF_INCLUDES=0 GENERATE_ERT_S_FUNCTION=0 INCLUDE_MDL_TERMINATE_FCN=1 COMBINE_OUTPUT_UPDATE_FCNS=1 MULTI_INSTANCE_CODE=0 INTEGER_CODE=0 S32DS_TARGET_DEFAULT_LCF=1 S32DS_TARGET_USER_LCF="MPC5744P_RAM.ld" GHS_TARGET_DEFAULT_LCF=1 GHS_TARGET_USER_LCF="MPC5744P_RAM.ld" DIAB_TARGET_DEFAULT_LCF=1 DIAB_TARGET_USER_LCF="MPC5744P_RAM.lin" ISPROTECTINGMODEL=NOTPROTECTING
Cleaning...
RELATIVE_PATH_TO_ANCHOR is ..
==== Removing object files from build directory ====
Copying necessary files to build directory...
Compiler details : "D:\Program Files\S32DS_Power_v2017R1/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-gcc" -DMPC574xP -mcpu=e200z4 -DSTART_FROM_FLASH --sysroot="D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2" -g3 -mbig -mvle -O3 -mregnames -mlsp -specs=ewl_c9x.specs -mhard-float -Wall -c -std=c99 -fdata-sections -ffunction-sections -fsigned-char -fmessage-length=0 -nostdinc -I. -I.. -I"D:\Program Files\Matlab2016a\simulink\include" -I"D:\Program Files\Matlab2016a\extern\include" -I"D:\Program Files\Matlab2016a\rtw\c\src" -I"D:\Program Files\Matlab2016a\rtw\c\libsrc" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\common" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\tcpip" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\serial" -I"D:\Program Files\Matlab2016a\rtw\c\src\ext_mode\custom" -I"D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2/EWL_C/include" -I"D:\Program Files\S32DS_Power_v2017R1/S32DS/e200_ewl2/EWL_C/include/pa" -ID:\PROGRA~1\MATLAB~1\simulink\include\sf_runtime -ID:\matlab_vcu\adc_ctu_dma_model_mbd_rtw -ID:\matlab_vcu -DUSE_RTMODEL -DMODEL=adc_ctu_dma_model -DREAL_T=float -DRT -DNUMST=1 -DTID01EQ=0 -DNCSTATES=0 -DMT=0 -DHAVESTDIO
Assembler details : "D:\Program Files\S32DS_Power_v2017R1/Cross_Tools/powerpc-eabivle-4_9/bin/powerpc-eabivle-as" -g3 -mbig -mvle -mregnames
Building assembly file crt0.o...
系统找不到指定的路径。
gmake: *** [crt0.o] Error 1
### Build procedure for model: 'adc_ctu_dma_model' aborted due to an error.
Build process completed successfully

0 件の賞賛
返信

4,806件の閲覧回数
jackjack
Contributor III
0 件の賞賛
返信

4,806件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello jackjack‌,

Thank you for installing our toolbox.

If you added the license file after you ran the mbd_pnt_path.m script, please set the Matlab path to default and rerun the script (in order to include the license in path). 

You can also try to change the extension from .lic to .dat.

Also, please follow this tutorial  Video Link : 7692.

Hope this helps,

Marius