Mklinux error on lsdk18.09

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mklinux error on lsdk18.09

2,057件の閲覧回数
ranga_yn
Contributor III

I am using LSDK flexbuild1809 on Ubuntu 18.04 running in a VirtualBox VM.

My target is LS2088ARDB.

I run the following command:

flex-builder -i autobuild-log -a arm64 -m ls2088ardb

INSTRUCTION: mklinux

DESTARCH: arm64

CONFIGLIST:build_lsdk.cfg

[sudo ] password for labadmin: //once given password

umount: mntrd: not mounted.

//And stopped is there any thing i can check to make sure my lsdk_linux_arm64_tiny.itb is generated.

ラベル(3)
0 件の賞賛
返信
1 返信

1,956件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hi [email protected]‌,

This community space do not cover the topic you need assistance on.

Please create new thread QorIQ Processing Platforms  on the community space OR new NXP support case according to following procedure:https://community.nxp.com/docs/DOC-329745

Hope this helps,

Marius

0 件の賞賛
返信