Memory write error if in subsystem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Memory write error if in subsystem

跳至解决方案
2,311 次查看
BillDuley
Contributor III

When utilizing the memory read / write blocks per the example project, things work great.

If I try to put the write block in a subsystem, I get the attached error:

BillDuley_0-1688070700051.png

My end goal is to write to a flash region and make the subsystem enabled to avoid memory wear out.

My blockset version is "Model-Based Design Toolbox for S32K3xx Series Version 1.2.2"

Is there a way around this error?

标记 (1)
0 项奖励
回复
1 解答
2,228 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hello @BillDuley ,

We have investigated the described issue and we would like to share with you the following fix, in the form of the check_range.p file contained by the archive attached to this post.

After you download the archive and extract the file, can you please copy it inside the <toolbox_root>/mbdtbx_s32k3/+mbd_s32k3/+mem folder and overwrite the already existing one? After this process is completed, you should be able to use a MBDT Memory Write block inside a subsystem, as required by your use case.

However, please note that this solution is applicable only for the current toolbox version you are using (1.2.2) and it will not work with newer toolbox versions due to compatibility issues.

Let us know if this helps or further assistance is needed from our side.

Thank you,
Irina

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,209 次查看
BillDuley
Contributor III

Patch worked great! Thx!

0 项奖励
回复
2,229 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hello @BillDuley ,

We have investigated the described issue and we would like to share with you the following fix, in the form of the check_range.p file contained by the archive attached to this post.

After you download the archive and extract the file, can you please copy it inside the <toolbox_root>/mbdtbx_s32k3/+mbd_s32k3/+mem folder and overwrite the already existing one? After this process is completed, you should be able to use a MBDT Memory Write block inside a subsystem, as required by your use case.

However, please note that this solution is applicable only for the current toolbox version you are using (1.2.2) and it will not work with newer toolbox versions due to compatibility issues.

Let us know if this helps or further assistance is needed from our side.

Thank you,
Irina

0 项奖励
回复