Matlab generated code on S32DS ARM 2.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Matlab generated code on S32DS ARM 2.2

2,934 次查看
saiello
Contributor I

Hello,

I get started to use NXP MBD tool for S32K142 with Matlab 2020b, I have created a simple model to test ADC and GPIO, I have build code on matlab downloading the code on the board without error. The problem is when I try to import the project on S32DS ARM 2.2 becouse I can't build code. Moreover I can't select the C/C++ Build window on project properties.   

Used tools:

NXP MDB toolbox 4.2.o

Matlab 2020b

S32DS ARM 2.2

Below I attach also the DS installation details.

0 项奖励
回复
0 回复数