Matlab generated code on S32DS ARM 2.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Matlab generated code on S32DS ARM 2.2

2,885件の閲覧回数
saiello
Contributor I

Hello,

I get started to use NXP MBD tool for S32K142 with Matlab 2020b, I have created a simple model to test ADC and GPIO, I have build code on matlab downloading the code on the board without error. The problem is when I try to import the project on S32DS ARM 2.2 becouse I can't build code. Moreover I can't select the C/C++ Build window on project properties.   

Used tools:

NXP MDB toolbox 4.2.o

Matlab 2020b

S32DS ARM 2.2

Below I attach also the DS installation details.

0 件の賞賛
返信
0 返答(返信)