MTRDEVKSPNK144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MTRDEVKSPNK144

1,679件の閲覧回数
aniket_bagade
Contributor III
  • what is difference between MTRDEVKSBNK144  and MTRDEVKSPNK144. I want development kit which has PMSM with HALL sensors. Which Should I prefer?
  • In both development kit NXP has used same motor though one kit is for BLDC and one is for PMSM.
0 件の賞賛
返信
1 返信

1,560件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi [email protected]‌

There is no HW difference between the 2 kits: PMSM vs BLDC

The HW hit itself is basically the same - same motor, same S32K144 and the same MotorGD shield.

There are 2 configuration differences when you order one or the other - depending on which one you order it comes pre-configured from factory with:

  1. The J9/J10 and J11 are set for measuring the phase currents (PMSM) or phase backEMF (BLDC)
  2. The MCU flash is pre-loaded with the PMSM or BLDC application code

Apart of those, there are no differences.

Hope this helps!

Daniel

0 件の賞賛
返信