MPC5748G:S32软件debug烧写不进去

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G:S32软件debug烧写不进去

1,500 Views
he_zhang
Contributor I

IMG_20191106_184949.jpgLoading programming algorithm . . .

WARNING - Selected .PCP file has been modified. CRC16 = $5A63

Done.

Programming sequency is : erase, blank check, program, and verify { default }

CMD>VC

Verifying object file CRC-16 to device ranges . . .

      block 00F90000-00F9001B  . . .

在使用软件debug调试时,烧写代码,卡在99%,上述为log,好像是芯片无法擦写了?

0 Kudos
Reply
1 Reply

1,333 Views
mariuslucianand
NXP Employee
NXP Employee

Hello 张 贺 ,

Do you generate the code using Model-Based Design Toolbox for MPC57xx? Because on this community we try to respond to questions related with the NXP's Simulink Toolbox and I've seen that your elf is called Debug_sample_boot_mcal_1M.elf.

Best Regards,

Marius 

0 Kudos
Reply