MPC5748G Dev Kit RevD CCP communication error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G Dev Kit RevD CCP communication error

Jump to solution
2,201 Views
swmurray
Contributor II

I'm getting started with Matlab/Simulnk MBDT examples with the following configuration:

MPC5748G Rev D Dev Kit

Model-Based Design Toolbox for MPC57xx Series Version 3.2.0

Matlab/SImulink R2020a

I have built the UART Hello World example but am getting a 'Loss Communication with CCP MCU' error when flashing.

I followed the mbd toolbox guide and installed everything okay, and have flashed rbf using S32DS successfully (AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx\tools\BootLoader\RBF_Files
MPC5748G_S32DS_UART2_CAN0.rbf).

I have confirmed the serial port settings in device manager and tried taking the *.mot file from the ***_rtw folder and programing it with the RAppID_BL.exe 

Also tried flasing the *.elf file directly from S32DS, rebooted and the RED Led was on, but nothing in the serial terminal (PuTTY) on the Com port (COM3)

I haven't been able to download the schematics for the board to check the serial port to see if the pin-out has changed from the revision used in the guide (Rev A); the link for the schematics doesn't work for some reason.

Running out of things to try so requesting some help / guidance 

Thanks in advance

 

 

swmurray_4-1645636861259.pngswmurray_4-1645636861259.png

 

swmurray_3-1645636849296.pngswmurray_3-1645636849296.png

 

swmurray_2-1645636666589.pngswmurray_2-1645636666589.png

 

swmurray_1-1645636651966.pngswmurray_1-1645636651966.png

swmurray_5-1645636955857.pngswmurray_5-1645636955857.png

swmurray_6-1645636996841.pngswmurray_6-1645636996841.png

 

Labels (1)
0 Kudos
Reply
1 Solution
2,110 Views
swmurray
Contributor II

Found the issue in the end - computer was too slow.

Time between pressing reset on dev board and it re-starting was too quick for RAppID to popup and detect the Boot Loader. 

View solution in original post

0 Kudos
Reply
1 Reply
2,111 Views
swmurray
Contributor II

Found the issue in the end - computer was too slow.

Time between pressing reset on dev board and it re-starting was too quick for RAppID to popup and detect the Boot Loader. 

0 Kudos
Reply