MPC5744P REV E1 : PIL simulation Error after flashing code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P REV E1 : PIL simulation Error after flashing code

Jump to solution
2,505 Views
sundarnatarajan
Contributor II

Hello,

I recently brought MPC5744P REV E1 board. 

I am using MATLAB 2016b, Toolbox 3.2.0.

I tried to run the example in MPC _Example -> common-.> Pil -> sim_pil_top_TC_mpc5744x. 

code gets generated, compiled, flashing starts with erasing and completes 100%.

Then error comes and stops. 

Error: "The Timeout of 10 seconds for receiving...." 

Am I missing something or ? Could someone help me out. 

Thanks in advance

0 Kudos
Reply
1 Solution
2,496 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @sundarnatarajan ,

 

Can you please check the pins configured in the Main Config Block? The PIL settings generate the code that initializes the UART driver. There are different instances used for the MPC5744P board. For RevE is the Serial 0, PB2 and PB3. Can you please check and select these pins?

mariuslucianand_0-1608304641352.pngmariuslucianand_0-1608304641352.png

Regards,

Marius

 

View solution in original post

Tags (1)
0 Kudos
Reply
2 Replies
2,497 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @sundarnatarajan ,

 

Can you please check the pins configured in the Main Config Block? The PIL settings generate the code that initializes the UART driver. There are different instances used for the MPC5744P board. For RevE is the Serial 0, PB2 and PB3. Can you please check and select these pins?

mariuslucianand_0-1608304641352.pngmariuslucianand_0-1608304641352.png

Regards,

Marius

 

Tags (1)
0 Kudos
Reply
2,403 Views
sundarnatarajan
Contributor II

Hello Marius,

Serial0 setting works. Great!!

thankyou for your timely reply.

Regards

Sundar N