MPC5744P REV E1 : PIL simulation Error after flashing code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5744P REV E1 : PIL simulation Error after flashing code

跳至解决方案
1,730 次查看
sundarnatarajan
Contributor II

Hello,

I recently brought MPC5744P REV E1 board. 

I am using MATLAB 2016b, Toolbox 3.2.0.

I tried to run the example in MPC _Example -> common-.> Pil -> sim_pil_top_TC_mpc5744x. 

code gets generated, compiled, flashing starts with erasing and completes 100%.

Then error comes and stops. 

Error: "The Timeout of 10 seconds for receiving...." 

Am I missing something or ? Could someone help me out. 

Thanks in advance

0 项奖励
回复
1 解答
1,721 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @sundarnatarajan ,

 

Can you please check the pins configured in the Main Config Block? The PIL settings generate the code that initializes the UART driver. There are different instances used for the MPC5744P board. For RevE is the Serial 0, PB2 and PB3. Can you please check and select these pins?

mariuslucianand_0-1608304641352.png

Regards,

Marius

 

在原帖中查看解决方案

标记 (1)
0 项奖励
回复
2 回复数
1,722 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @sundarnatarajan ,

 

Can you please check the pins configured in the Main Config Block? The PIL settings generate the code that initializes the UART driver. There are different instances used for the MPC5744P board. For RevE is the Serial 0, PB2 and PB3. Can you please check and select these pins?

mariuslucianand_0-1608304641352.png

Regards,

Marius

 

标记 (1)
0 项奖励
回复
1,628 次查看
sundarnatarajan
Contributor II

Hello Marius,

Serial0 setting works. Great!!

thankyou for your timely reply.

Regards

Sundar N