MPC5744P REV E1 : PIL simulation Error after flashing code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P REV E1 : PIL simulation Error after flashing code

ソリューションへジャンプ
2,578件の閲覧回数
sundarnatarajan
Contributor II

Hello,

I recently brought MPC5744P REV E1 board. 

I am using MATLAB 2016b, Toolbox 3.2.0.

I tried to run the example in MPC _Example -> common-.> Pil -> sim_pil_top_TC_mpc5744x. 

code gets generated, compiled, flashing starts with erasing and completes 100%.

Then error comes and stops. 

Error: "The Timeout of 10 seconds for receiving...." 

Am I missing something or ? Could someone help me out. 

Thanks in advance

0 件の賞賛
返信
1 解決策
2,569件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @sundarnatarajan ,

 

Can you please check the pins configured in the Main Config Block? The PIL settings generate the code that initializes the UART driver. There are different instances used for the MPC5744P board. For RevE is the Serial 0, PB2 and PB3. Can you please check and select these pins?

mariuslucianand_0-1608304641352.png

Regards,

Marius

 

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
2 返答(返信)
2,570件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @sundarnatarajan ,

 

Can you please check the pins configured in the Main Config Block? The PIL settings generate the code that initializes the UART driver. There are different instances used for the MPC5744P board. For RevE is the Serial 0, PB2 and PB3. Can you please check and select these pins?

mariuslucianand_0-1608304641352.png

Regards,

Marius

 

タグ(1)
0 件の賞賛
返信
2,476件の閲覧回数
sundarnatarajan
Contributor II

Hello Marius,

Serial0 setting works. Great!!

thankyou for your timely reply.

Regards

Sundar N