MPC5744P FreeMASTER Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P FreeMASTER Error

ソリューションへジャンプ
3,289件の閲覧回数
260068845
Contributor III

Hello,


     I refer to the FreeMASTER Interface in Chapter 8 of the MPC5744P document "Model-Based Design Toolbox User Manual" for FreeMASTER testing. However, after I finished those steps, I am getting an error when compiling. The error message is as shown below. What is the problem? What? The engineering documentation is in the attachment, thank you for your answers.

捕获.PNG

0 件の賞賛
返信
1 解決策
3,190件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Did you have an earlier version of the toolbox installed? To be sure, can you try and reset the MATLAB path? For that you should go to MATLAB Home tab -> Set Path -> Click on Default -> Then click on Save.

Capture.JPG

Untitled.png

and then run the mbd_mpc_path script so you install the path for the toolbox over a fresh, default MATLAB path. 

 

Note: you will lose other paths other than the default + MPC toolbox paths by doing this. Consider saving the current  contents of your MATLAB path (you can get it by typing matlabpath in the MATLAB terminal for instance).

 

Note: this file is located in {INSTALL_ROOT}/src.

I'm asking this because I cannot replicate the issue you are having - but I can get an error using some older tlc files in conjunction with the new toolbox (the one that you have installed). This is the reason why I assume this to be the problem. Please let me know if this does the trick.

 

Kind regards,

Razvan.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,190件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Could you confirm that you are using version 3.0.0 of our MPC toolbox? And also could you run the following command in MATLAB terminal and share the output with me?

ver

I could not reproduce your error, thus I'm thinking maybe you have files from previous version of the MPC toolbox shadowing the ones from v3.0.0. 

Kind regards,

Razvan.

0 件の賞賛
返信
3,190件の閲覧回数
260068845
Contributor III

Hello,constantinrazvan.chivu‌

   I sure the version of the MPC toolbox is v3.00.

pastedImage_1.pngpastedImage_2.png

0 件の賞賛
返信
3,191件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Did you have an earlier version of the toolbox installed? To be sure, can you try and reset the MATLAB path? For that you should go to MATLAB Home tab -> Set Path -> Click on Default -> Then click on Save.

Capture.JPG

Untitled.png

and then run the mbd_mpc_path script so you install the path for the toolbox over a fresh, default MATLAB path. 

 

Note: you will lose other paths other than the default + MPC toolbox paths by doing this. Consider saving the current  contents of your MATLAB path (you can get it by typing matlabpath in the MATLAB terminal for instance).

 

Note: this file is located in {INSTALL_ROOT}/src.

I'm asking this because I cannot replicate the issue you are having - but I can get an error using some older tlc files in conjunction with the new toolbox (the one that you have installed). This is the reason why I assume this to be the problem. Please let me know if this does the trick.

 

Kind regards,

Razvan.

0 件の賞賛
返信
3,190件の閲覧回数
260068845
Contributor III

Helloconstantinrazvan.chivu‌,

      According to your method,I can build my model successfully. Thank you very much. 

Best regards,

Zewu

0 件の賞賛
返信