MPC5675K Simulink code generation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5675K Simulink code generation error

2,017件の閲覧回数
AsierMaser
Contributor II

Hi all,

I am working on a Simulink software and I am getting an error when generating the code. It is strange because both the compiler and the code generator advisor say that there is no error in the code, but the Matlab prompt shows an error message. This is what I get in the Matlab prompt:

Sin título.pngSin título.png

As I have said, the compiler shows no error, but the code generator advisor  shows a warning. The warning is regarding the use of pulse generator blocks, and it is the only warning as you can see in the attached figure:

Sin título.pngSin título.png

I also attach the config of the realtime workshop config page:

Sin título.pngSin título.png

My system info:

Windows XP SP3 32 bits

Matlab R2010a 

Motor Control Toolbox for MPC567xK

Any idea on what is happening here?

Best regards

0 件の賞賛
返信
2 返答(返信)

1,973件の閲覧回数
SorinIBancila
NXP Employee
NXP Employee

Hello,

Unfortunately the toolbox you are trying to use is deprecated and I am unable to properly provide support for it. 

A suggestion I have for you is to consult the Motor_Control_Toolbox_Manual included in the toolbox and to make sure you followed all the steps required (Chapter 2.2 Installation Steps and 4. Required and Recommended Products).

Best regards,

Bancila Sorin

0 件の賞賛
返信

1,961件の閲覧回数
AsierMaser
Contributor II

Hello,

We were able to solve the problem, now code generation works as expected.

Best regards

0 件の賞賛
返信