MPC564xL Motor Control Toolbox patch for Matlab/Simulink 2017b

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC564xL Motor Control Toolbox patch for Matlab/Simulink 2017b

2,804件の閲覧回数
mcgillformulael
Contributor I

Hello,

We are having trouble with the hardware implementation of our MPC564xL with Matlab & Simulink R2017b. Indeed, our Motor Control Toolbox Hardware Implementation blocks are not compatible with R2017b, and return errors when trying to generate code with Simulink. See picture attached. As seen, even the simplest model leads to an error when trying to generate code. "Undefined function 'slsfnagctlr' for input arguments of type 'char'." 

Therefore, I wanted to know if this is an issue that can be fixed? I have seen the same issue on the Community Forum but with a different Microprocessor. Would it be possible to fix the issue also on the MPC564xl?

Kind Regards,

Michael

McGill Formula Electric

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,364件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hi mcgillformulaelectric‌,

I've created HotFix_1 for this. Can you please try it and confirm that it works for you?

Thank you,

Paul

0 件の賞賛
返信

2,364件の閲覧回数
mcgillformulael
Contributor I

Hi paulvlase‌,

Thank you for your excellent support. The patch did work!

Best,

Michael

0 件の賞賛
返信